This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-OMAPL138: IPC example

Part Number: PROCESSOR-SDK-OMAPL138
Other Parts Discussed in Thread: TMS320C6748, OMAPL138, OMAP-L138

Hello,

I am already developed a data logger using TMS320C6748 DSP processor. I used processor sdk in windows laptop with code composer studio 8. Also I am able to put my application in boot.

Now I need to replace the TMS320C6748 with OMAPL138 processor, I need to run applications running in  ARM and DSP separately and  data should transferred between the processors using IPC.

Can I do this using the windows laptop with code composer studio 8? or I require a Linux laptop to program ARM processor with linux os installed?

Is there any document available for this so that I can follow the steps.

Thanks & regards

Navaneetha krishnan