Respected sir,
I am trying to add SPI to my yocto image. I found the following link which was useful.
But here i am confused about where to find the files which needs to be changed. I want to modify the bbb-4dcape70t.dtb from ROOT/boot/ to add SPI.
So where to find the bbb-4dcape70t.dts file which i can modify??
Where to find the file to set "CONFIG_SPI_SPIDEV=y"??
Do i need to change my kernal-recipe?? If yes where to find .bbappend file (linux-ti-staging-4.4.bbappend)??
If there are any other changes I need to do add SPI please suggest.
Regards,
Digvijay