Part Number: AM5728
I copy the paltform file am57xx-evm to am57xx-myboard and change it ike following:
armv7l dra7xx am57xx-myboard
but there is so many errors:
<<<test_start>>> tag=VIDEO_S_FUNC_GST_MPEG4_480P stime=1562477083 cmdline="source 'common.sh'; do_cmd 'gst.sh -d "M4V/HistoryOfTI-480p.m4v" -c "mpeg4" -r "480p"'" contacts="" analysis=exit <<<test_output>>> |TRACE LOG|Inside do_cmd:CMD=gst.sh -d "M4V/HistoryOfTI-480p.m4v" -c "mpeg4" -r "480p"| Demo file /usr/share/ti/video/HistoryOfTI-480p.m4v exists |TRACE LOG|Inside do_cmd:CMD=gst-launch-1.0 playbin uri=file:///usr/share/ti/video/HistoryOfTI-480p.m4v video-sink="kmssink" audio-sink="alsasink"| Setting pipeline to PAUSED ... ERROR: Pipeline doesn't want to pause. ERROR: from element /GstAlsaSink:alsasink0: Could not open audio device for playback. Additional debug info: ../../../gst-plugins-base-1.14.4/ext/alsa/gstalsasink.c(865): gst_alsasink_open (): /GstAlsaSink:alsasink0: Playback open error on device 'default': No such file or directory Setting pipeline to NULL ... Freeing pipeline ... |ERROR|Line: File:gst-launch-1.0 playbin uri=file:///usr/share/ti/video/HistoryOfTI-480p.m4v video-sink="kmssink" audio-sink="alsasink" failed. Return code is 255 - | |ERROR|Line: File:gst.sh -d "M4V/HistoryOfTI-480p.m4v" -c "mpeg4" -r "480p" failed. Return code is 255 - | <<<execution_status>>> initiation_status="ok" duration=0 termination_type=exited termination_id=255 corefile=no cutime=12 cstime=2 <<<test_end>>>
So, what'this? How does the runltp use the platform file to decide the test?