Hi,
I have an issue while compiling kernel sources. Actually, i did clean and then tried to rebuild the kernel. I am working on DRA71X and SDK 3.04. When I tried to build, issuing command "bitbake -c compile -f linux-ti-staging" I got this below error:
WARNING: linux-ti-staging-4.4.45+gitAUTOINC+89944627d5-r1a.arago5 do_fetch: Failed to fetch URL git://git.omapzoom.org/kernel/omap;protocol=git;branch=p-ti-lsk-linux-4.4.y-next, attempting MIRRORS if available
ERROR: linux-ti-staging-4.4.45+gitAUTOINC+89944627d5-r1a.arago5 do_fetch: Fetcher failure: Fetch command failed with exit code 128, output:
Cloning into bare repository '/mnt/yocto/yocto_repo/downloads/git2/git.omapzoom.org.kernel.omap'...
fatal: read error: Connection reset by peer
ERROR: linux-ti-staging-4.4.45+gitAUTOINC+89944627d5-r1a.arago5 do_fetch: Function failed: Fetcher failure for URL: 'git://git.omapzoom.org/kernel/omap;protocol=git;branch=p-ti-lsk-linux-4.4.y-next'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /mnt/yocto/yocto_repo/build/arago-tmp-external-linaro-toolchain/work/delphi_jlr_isp_proto-linux-gnueabi/linux-ti-staging/4.4.45+gitAUTOINC+89944627d5-r1a.arago5/temp/log.do_fetch.59891
ERROR: Task 0 (/mnt/yocto/yocto_repo/sources/meta-ti/recipes-kernel/linux/linux-ti-staging_4.4.bb, do_fetch) failed with exit code '1'
Please help with this.
regards,
Harish.