Other Parts Discussed in Thread: OMAP-L138, SYSBIOS, OMAPL138, TMS320C6748
Hello,
I'm trying to build an initial 6.30 SYSBIOS project for my OMAP-L138 6748 DSP, using CCS V4.2. I followed the steps in the "Sys/BIOS 6.30 Getting Started Guide". And I can build the example SWI project using the procedure documented there. However, when going to load the resulting output file to the DSP on the OMP-L138, I get the following error:
"C674X_0: File Loader: Data verification failed at address 0xC1010430 Please verify target memory and memory map.
Error found during data verification.
Ensure the linker command file matches the memory map."
I've tried a few things to resolve this, but with no luck. Any pointers would be greatly appreciated.
I haven't added any linker command file to the project, but am wondering if I should.
Regards,
Robert