This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3354: 36MHz SPI clock

Expert 4716 points

Part Number: AM3354

Hi team,

Is it possible to set SPI clock to 36MHz? If yes, how?

I am using 24MHz crystal.

  • Hi,

    The McSPI functional clock is 48MHz, generated by the fixed /4 divider in the PRCM from the 192MHz Peripheral PLL output clock (AM335x TRM Rev. P section 8.1.6.8). To change to 36MHz, you will need to set the Peripheral PLL to 144MHz, which will affect the proper functioning of all other peripherals clocked by it. In short, this is not possible.