Part Number: TDA2SX
Hello all,
We are working on a custom board based on tda2sx.After connecting a SATA SSD we are getting the following errors,
ata1: irq_stat 0x00000040, connection status changed
ata1: SError: { CommWake DevExch }
ata1: hard resetting link
ata1: SATA link down (SStatus 1 SControl 300)
ata1: EH complete
ata1: exception Emask 0x10 SAct 0x0 SErr 0x4040000 action 0xe frozen
ata1: irq_stat 0x00000040, connection status changed
ata1: SError: { CommWake DevExch }
ata1: hard resetting link
ata1: SATA link down (SStatus 1 SControl 300)
ata1: EH complete
ata1: exception Emask 0x10 SAct 0x0 SErr 0x4040000 action 0xe frozen
ata1: irq_stat 0x00000040, connection status changed
ata1: SError: { CommWake DevExch }
ata1: limiting SATA link speed to 1.5 Gbps
ata1: hard resetting link
ata1: SATA link up 1.5 Gbps (SStatus 113 SControl 310)
ata1.00: ATA-9: SED2FV-MT SATA SSD 256GB, R0411D, max UDMA/133
ata1.00: 494927872 sectors, multi 1: LBA48 NCQ (depth 31/32)
ata1.00: configured for UDMA/133
ata1: EH complete
scsi 0:0:0:0: Direct-Access ATA SED2FV-MT SATA S 1D PQ: 0 ANSI: 5
sd 0:0:0:0: [sdb] 494927872 512-byte logical blocks: (253 GB/236 GiB)
sd 0:0:0:0: Attached scsi generic sg1 type 0
sd 0:0:0:0: [sdb] Write Protect is off
sd 0:0:0:0: [sdb] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA
sdb: sdb1
sd 0:0:0:0: [sdb] Attached SCSI disk
ata1.00: exception Emask 0x10 SAct 0x400000 SErr 0x280100 action 0x6 frozen
ata1.00: irq_stat 0x08000000, interface fatal error
ata1: SError: { UnrecovData 10B8B BadCRC }
ata1.00: failed command: READ FPDMA QUEUED
ata1.00: cmd 60/08:b0:b0:fd:7f/00:00:1d:00:00/40 tag 22 ncq 4096 in
res 40/00:b0:b0:fd:7f/00:00:1d:00:00/40 Emask 0x10 (ATA bus error)
ata1.00: status: { DRDY }
ata1: hard resetting link
ata1: SATA link up 1.5 Gbps (SStatus 113 SControl 310)
ata1.00: configured for UDMA/133
ata1: EH complete
ata1.00: exception Emask 0x10 SAct 0x200000 SErr 0x280100 action 0x6 frozen
ata1.00: irq_stat 0x08000000, interface fatal error
ata1: SError: { UnrecovData 10B8B BadCRC }
ata1.00: failed command: READ FPDMA QUEUED
ata1.00: cmd 60/f0:a8:10:01:00/00:00:00:00:00/40 tag 21 ncq 122880 in
res 40/00:a8:10:01:00/00:00:00:00:00/40 Emask 0x10 (ATA bus error)
ata1.00: status: { DRDY }
What could be the issue?
Regards,
Murugan S