This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMIC110: AMIC ICE schematics

Part Number: AMIC110
Other Parts Discussed in Thread: SN74LVC2G66

Hi there

Since I also want to connect two PHYS for Ethercat to the AMIC110, I looked at the circuit and the software for the EVAL board. I do not quite understand the purpose of U10 (SN74LVC2G66). After configuring the PHYs and two AMIC pins as input, this IC will switch the RX_CLK and the PHY_LED1. Why is that necessary, can't the AMIC boot from the SPI first, then confirure the two AMIC pins
as inputs (for RX_CLK and PHY_LED1) and then finally release the PHY from the reset? Can't U10 be omited in that case?

best regards

Thomas