Dears:
There happens the failure of Vector.push_back, pls. refer the below picture:
Btw: There will happen the issue using DSP/BIOS, if not using BIOS the program(C++ Add STL) is OK.
compiler: TIC6000 V7.4.4
CPU: TMS320C6748
Tool:CCS5.5
Dsp/bios: 5.4.2
File format: COFF
The begin pointer: 0x00000000