#1. I would like to go through the uboot source code. where is the main function source file?
arch/arm/cpu/armv7/start.S
/*
* Setup vector:
* (OMAP4 spl TEXT_BASE is not 32 byte aligned.
* Continue to use ROM code vector only in OMAP4 spl)
*/
#if !(defined(CONFIG_OMAP44XX) && defined(CONFIG_SPL_BUILD))
/* Set V=0 in CP15 SCTLR register - for VBAR to point to vector */
mrc p15, 0, r0, c1, c0, 0 @ Read CP15 SCTLR Register
bic r0, #CR_V @ V = 0
mcr p15, 0, r0, c1, c0, 0 @ Write CP15 SCTLR Register
/* Set vector address in CP15 VBAR register */
ldr r0, =_start
mcr p15, 0, r0, c12, c0, 0 @Set VBAR
#endif
/* the mask ROM code should have PLL and others stable */
#ifndef CONFIG_SKIP_LOWLEVEL_INIT
bl cpu_init_cp15
#ifndef CONFIG_SKIP_LOWLEVEL_INIT_ONLY
bl cpu_init_crit
#endif
#endif
bl _main
#2. Is there a poring guide as that of old SDK in below page? or Will it be updated according to new version Processor SDK?
#3. How to boot custom board with the default uboot, which function which macro definition to modify?