Dear all:
when i call ALG_vidDecRun , sometime occur error as below:
1.
ERROR (alg_vidDec.c|ALG_vidDecRun|303): status=-1
ERROR (alg_vidDec.c|ALG_vidDecRun|310): XDM_GETSTATUS failed with error code = 0x4f , status=-1
2.
VIDDEC2_OutArgs.displayBufs[0].bufDesc[0].buf is NULL
Dose anyone know what's that meanning above two case.
In addition , i play the same file .
Above two case sometimes appear , sometimes not appear .
This make me feel confused.
Should i adjust the parameter of the encode or the decoder.
Thanks you for your visit
Best regard