Other Parts Discussed in Thread: OMAP3530
Hello,
I am having sbc8100 board which uses the OMAP 3530 arch.. The Linux kernel that came with the board had 2.6.29 version of the kernel.My main motive was to build QT for this board using the graphics SDK provided by your site.
Compiling the Graphics SDK required me to download the latest PSP from the site,which I did.Now after fixing all the issues in the compilation I am able to cross compile it.Now comes the part in which I would have to put the execs on the board and try to run the examples and the demos..MY question is what changes are reqd for the kernel as the version on the board is 2.6.29 and the PSP contained 2.6.32
Are there any more changes expected ?
Thanks,
Anand