This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDK 5515

Hai,

            I have purchased the TMS320C5515FDK. I need some clarifications in that board,someone please help me out in this....

The CD along with this bundle is only having some example codes and gel files. So which version of CCS will i suppose to program or to execute the codes comes along with the CD.

What is the emulator i have to use, please give me the details and the emulator compatibility with CCS.  

I am having two numbers among that one kit have some problem that stand alone example(Swipe sensor example) was not working, In another kit it is working, I hope it is programed in flash memory, so tell me how to do the flash program in that board,

Thanks in advance......

  • Since the demo codes are source codes, you can use either CCS4 or CCS3.3.

    The package provides a mini converter for JTAG emulator, any emulators support that should work. I use an USB560 emulator from Blackhawk, but i know people using emulators from Spectrum Digital.

    The connector for the swipe sensor is so small, have use try reinsert it or swap it with the working one?