Other Parts Discussed in Thread: AM3517
Hello,
Our board with a AM3517 (XAM3517 on the board now) has a Samsung NAND K9F1G08 (Samsung NAND device ID: 0xec, 0xF1, 0x00, 0x95, 0x40 128MiB 3,3V 8-bit))
connected on CS0.
from CCS we launch X-loader : X-loader starts ... loads u-boot ... loads kernel and so on.
but at power on the ROM boot does not load x-loader.
The x-loader has been loaded in the flash as shown in the PSP documentation from x-loader.bin.ifl with size and load address in the first locations.
Did I something wrong?
Thanks for help