This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320DM8167: Power requirements

Part Number: TMS320DM8167

Hi Team,

Please help me answer the follow question from my customer, thank you so much.

1. What are the power requirements for TMS320DM8167?
    Are there any requirements regarding ripple voltage for each power supply used?
2. The TMS320DM8167 microcontroller requires a power supply sequence. I input 3.3V first. Is it possible that 3.3V will sneak into the 1.8V power supply?

Best Regards,
Tom Liu

  • Hi Liu,

    Liu Yang said:
    1. What are the power requirements for TMS320DM8167?

    These are described in DM816x datasheet. You can also check below pointers:

    Liu Yang said:
    Are there any requirements regarding ripple voltage for each power supply used?

    We have "Dynamic noise at VDDA_PLL pins" of MAX 50 mV p-p, check datasheet section 8.3.4.2 PLL Power Supply Filtering

    We have only MIN, NOM and MAX voltage for each power supply. Check datasheet section 5.3 Recommended Operating Conditions

     

    Liu Yang said:
    2. The TMS320DM8167 microcontroller requires a power supply sequence. I input 3.3V first. Is it possible that 3.3V will sneak into the 1.8V power supply?

    As you are aligned with DM816x power sequence (3.3V first), this should NOT be possible.

     

    Regards,
    Pavel