This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2P-ACD: Linux - VSDK IPC and Message Que

Part Number: TDA2P-ACD

Hi all,

I have some usecase with different links. Some of them are running on RTOS (IPU2, DPS, EVE) and some of them on Linux (A15). So, after few hours, Linux just hangs, terminal is not responsive, but camera is still working (IPU core). I read on some post on forum that VSDK IPC method and Linux message que method can not co-exist. It is related to rpmsg driver. So, can you confirm that this is correct and it could be cause of this problem.

Best regards,

Stefan.

  • Hi,

    One more information about this issue. After linux hangs and when killing apps.out with CTRL + C, I'm receiving following message:

    [14111.130217] virtio_rpmsg_bus virtio2: msg received with no recipient

    Best regards,

    Stefan.

  • Hi Stefan,

    Can you please let us know which SDK and what IPC methods are being used on Linux (A15) to communicate between which cores? Are you using MessageQ for communication between Linux and a remote core at the same time you are using links between Linux (A15) and the same remote core?

    If there are issues with configuration related to using MessageQ and another IPC on Linux (A15) for communication to a remote core, they would show up at startup time as one method would fail to initialize communication. Are you seeing the failure at initialization time?

    Regarding the "msg received with no recipient" trace, that will happen when there is no endpoint to receive a message sent to Linux (A15) by the remote core. If the remote core is still sending messages to A15, but the Linux application has been killed and closed it's rpmsg connection (endpoint), then this trace would be seen.

    Thanks,

    Angela