This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: U-boot customization

Part Number: AM5728

Hi,

I have updated the mux_data.h and the board.c(for the EMIF data).

Question 1: I have just copied the EMIF tool Output (c source code) to the board.c..........Is it fine or i need to change some code?

Question 2:How i can compile these file?

Question 2:How i can create the u-boot.img and the MLO files for the uboot sd card.? I need the details and the commands.

Thanks