This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA3XEVM: How RDM is generated and the energy is calculated by CFAR for CUT

Part Number: TDA3XEVM

1. We compared the RDM directly output from TI board and the RDM generated by applying  2D-FFT to raw ADC data divided by 16, and found that the elements of the former is much less than the latter. Could you elaborate on how  RDM is generated by TI? Is  the value of RDM elements in log2 domain?

2. In the CFAR  detection list ouptut from TI board, there are indices of Doppler and range bins and the associated energy (see attachment). I used the indices of the detected bins and found that the energy is quite different from that shown in detection list. How is the energy of the detection list calculated ?

3. How are the multiple channels combined to do CFAR? Noncoherently combining, i.e., log2(abs(rdm_0).^2+...+abs(rdm_N).^2)?

RadarMode - 1, NumOfDets - 1475
Frame 12: VelIdx:   0, Velocity -  0.00 m/s, RangeIdx:  33, Range -  42.57 m, Energy - 2912
Frame 12: VelIdx:   0, Velocity -  0.00 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 3961
Frame 12: VelIdx:   0, Velocity -  0.00 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 4827
Frame 12: VelIdx:   0, Velocity -  0.00 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 5105
Frame 12: VelIdx:   0, Velocity -  0.00 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 4824
Frame 12: VelIdx:   0, Velocity -  0.00 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 3883
Frame 12: VelIdx:   1, Velocity -  0.58 m/s, RangeIdx:  33, Range -  42.57 m, Energy - 2633
Frame 12: VelIdx:   1, Velocity -  0.58 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 3671
Frame 12: VelIdx:   1, Velocity -  0.58 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 4527
Frame 12: VelIdx:   1, Velocity -  0.58 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 4808
Frame 12: VelIdx:   1, Velocity -  0.58 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 4527
Frame 12: VelIdx:   1, Velocity -  0.58 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 3589
Frame 12: VelIdx:   2, Velocity -  1.16 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 2785
Frame 12: VelIdx:   2, Velocity -  1.16 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 3632
Frame 12: VelIdx:   2, Velocity -  1.16 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 3903
Frame 12: VelIdx:   2, Velocity -  1.16 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 3627
Frame 12: VelIdx:   2, Velocity -  1.16 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 2685
Frame 12: VelIdx:   3, Velocity -  1.74 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 2121
Frame 12: VelIdx:  33, Velocity - 19.14 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5136
Frame 12: VelIdx:  33, Velocity - 19.14 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 6029
Frame 12: VelIdx:  33, Velocity - 19.14 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6308
Frame 12: VelIdx:  33, Velocity - 19.14 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6033
Frame 12: VelIdx:  33, Velocity - 19.14 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 5136
Frame 12: VelIdx:  34, Velocity - 19.72 m/s, RangeIdx:  33, Range -  42.57 m, Energy - 4849
Frame 12: VelIdx:  34, Velocity - 19.72 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5419
Frame 12: VelIdx:  34, Velocity - 19.72 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 5444
Frame 12: VelIdx:  34, Velocity - 19.72 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 4989
Frame 12: VelIdx:  34, Velocity - 19.72 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 4107
Frame 12: VelIdx:  35, Velocity - 20.30 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 3965
Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  33, Range -  42.57 m, Energy - 4318
Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5216
Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 6033
Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6305
Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6017
Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 5039
Frame 12: VelIdx:  38, Velocity - 22.04 m/s, RangeIdx:  33, Range -  42.57 m, Energy - 4937
Frame 12: VelIdx:  38, Velocity - 22.04 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5434
Frame 12: VelIdx:  38, Velocity - 22.04 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 5444
Frame 12: VelIdx:  38, Velocity - 22.04 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 4960
Frame 12: VelIdx:  41, Velocity - 23.78 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 6037
Frame 12: VelIdx:  41, Velocity - 23.78 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6305
Frame 12: VelIdx:  41, Velocity - 23.78 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6022
Frame 12: VelIdx:  41, Velocity - 23.78 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 5077
Frame 12: VelIdx:  45, Velocity - 26.10 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6308
Frame 12: VelIdx:  49, Velocity - 28.42 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6308
Frame 12: VelIdx:  53, Velocity - 30.74 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 6013
Frame 12: VelIdx:  53, Velocity - 30.74 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6301
Frame 12: VelIdx:  53, Velocity - 30.74 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6033
Frame 12: VelIdx:  54, Velocity - 31.32 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5424
Frame 12: VelIdx:  54, Velocity - 31.32 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 5458
Frame 12: VelIdx:  57, Velocity - 33.06 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5188
Frame 12: VelIdx:  57, Velocity - 33.06 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 6041
Frame 12: VelIdx:  57, Velocity - 33.06 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6308
Frame 12: VelIdx:  57, Velocity - 33.06 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6029
Frame 12: VelIdx:  57, Velocity - 33.06 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 5105
Frame 12: VelIdx:  58, Velocity - 33.64 m/s, RangeIdx:  33, Range -  42.57 m, Energy - 4886
Frame 12: VelIdx:  58, Velocity - 33.64 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5429
Frame 12: VelIdx:  58, Velocity - 33.64 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 5434
Frame 12: VelIdx:  58, Velocity - 33.64 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 4946
Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  33, Range -  42.57 m, Energy - 4026
Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5178
Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 6033
Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6308
Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6033
Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 5114
Frame 12: VelIdx:  62, Velocity - 35.96 m/s, RangeIdx:  33, Range -  42.57 m, Energy - 4811
Frame 12: VelIdx:  62, Velocity - 35.96 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5392
Frame 12: VelIdx:  62, Velocity - 35.96 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 5429
Frame 12: VelIdx:  62, Velocity - 35.96 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 4977
Frame 12: VelIdx:  63, Velocity - 36.54 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 3873
Frame 12: VelIdx:  33, Velocity - 19.14 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5136
Frame 12: VelIdx:  33, Velocity - 19.14 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 6029
Frame 12: VelIdx:  33, Velocity - 19.14 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6308
Frame 12: VelIdx:  34, Velocity - 19.72 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5419
Frame 12: VelIdx:  34, Velocity - 19.72 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 5444
Frame 12: VelIdx:  34, Velocity - 19.72 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 4989
Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5216
Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 6033
Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6305
Frame 12: VelIdx:  38, Velocity - 22.04 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5434
Frame 12: VelIdx:  38, Velocity - 22.04 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 5444
Frame 12: VelIdx:  38, Velocity - 22.04 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 4960
Frame 12: VelIdx:  41, Velocity - 23.78 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5220
Frame 12: VelIdx:  41, Velocity - 23.78 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 6037
Frame 12: VelIdx:  41, Velocity - 23.78 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6305
Frame 12: VelIdx:  45, Velocity - 26.10 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6308
Frame 12: VelIdx:  49, Velocity - 28.42 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6308
Frame 12: VelIdx:  53, Velocity - 30.74 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 6013
Frame 12: VelIdx:  53, Velocity - 30.74 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6301
Frame 12: VelIdx:  54, Velocity - 31.32 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5424
Frame 12: VelIdx:  54, Velocity - 31.32 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 5458
Frame 12: VelIdx:  57, Velocity - 33.06 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5188
Frame 12: VelIdx:  57, Velocity - 33.06 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 6041
Frame 12: VelIdx:  57, Velocity - 33.06 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6308
Frame 12: VelIdx:  58, Velocity - 33.64 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5429
Frame 12: VelIdx:  58, Velocity - 33.64 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 5434
Frame 12: VelIdx:  58, Velocity - 33.64 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 4946
Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5178
Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 6033
Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6308
Frame 12: VelIdx:  62, Velocity - 35.96 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5392
Frame 12: VelIdx:  62, Velocity - 35.96 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 5429
Frame 12: VelIdx:  62, Velocity - 35.96 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 4977
Frame 12: VelIdx:  33, Velocity - 19.14 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6033
Frame 12: VelIdx:  34, Velocity - 19.72 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 4107
Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6017
Frame 12: VelIdx:  41, Velocity - 23.78 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6022
Frame 12: VelIdx:  53, Velocity - 30.74 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6033
Frame 12: VelIdx:  57, Velocity - 33.06 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6029
Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6033
Frame 12: VelIdx:  62, Velocity - 35.96 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 3974
Frame 12: VelIdx:  97, Velocity - 19.14 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5467
Frame 12: VelIdx:  97, Velocity - 19.14 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 6363
Frame 12: VelIdx:  97, Velocity - 19.14 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6647
Frame 12: VelIdx:  97, Velocity - 19.14 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6369
Frame 12: VelIdx:  97, Velocity - 19.14 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 5449
Frame 12: VelIdx:  98, Velocity - 19.72 m/s, RangeIdx:  33, Range -  42.57 m, Energy - 5036
Frame 12: VelIdx:  98, Velocity - 19.72 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5626
Frame 12: VelIdx:  98, Velocity - 19.72 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 5643
Frame 12: VelIdx:  98, Velocity - 19.72 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 5089
Frame 12: VelIdx:  99, Velocity - 20.30 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 4257
Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  33, Range -  42.57 m, Energy - 4757
Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5558
Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 6373
Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6644
Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6360
Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 5367
Frame 12: VelIdx: 102, Velocity - 22.04 m/s, RangeIdx:  33, Range -  42.57 m, Energy - 5043
Frame 12: VelIdx: 102, Velocity - 22.04 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5620
Frame 12: VelIdx: 102, Velocity - 22.04 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 5626
Frame 12: VelIdx: 102, Velocity - 22.04 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 5013
Frame 12: VelIdx: 105, Velocity - 23.78 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5544
Frame 12: VelIdx: 105, Velocity - 23.78 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 6369
Frame 12: VelIdx: 105, Velocity - 23.78 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6644
Frame 12: VelIdx: 105, Velocity - 23.78 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6357
Frame 12: VelIdx: 105, Velocity - 23.78 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 5364
Frame 12: VelIdx: 109, Velocity - 26.10 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6644
Frame 12: VelIdx: 109, Velocity - 26.10 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6353
Frame 12: VelIdx: 113, Velocity - 28.42 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6638
Frame 12: VelIdx: 113, Velocity - 28.42 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6357
Frame 12: VelIdx: 117, Velocity - 30.74 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6644
Frame 12: VelIdx: 117, Velocity - 30.74 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6373
Frame 12: VelIdx: 121, Velocity - 33.06 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6650
Frame 12: VelIdx: 121, Velocity - 33.06 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6366
Frame 12: VelIdx: 125, Velocity - 35.38 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6647
Frame 12: VelIdx: 125, Velocity - 35.38 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6363
Frame 12: VelIdx:  95, Velocity - 17.98 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 4385
Frame 12: VelIdx:  97, Velocity - 19.14 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5467
Frame 12: VelIdx:  97, Velocity - 19.14 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 6363
Frame 12: VelIdx:  97, Velocity - 19.14 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6647
Frame 12: VelIdx:  98, Velocity - 19.72 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5626
Frame 12: VelIdx:  98, Velocity - 19.72 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 5643
Frame 12: VelIdx:  98, Velocity - 19.72 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 5089
Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5558
Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 6373
Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6644
Frame 12: VelIdx: 102, Velocity - 22.04 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5620
Frame 12: VelIdx: 102, Velocity - 22.04 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 5626
Frame 12: VelIdx: 105, Velocity - 23.78 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 6369
Frame 12: VelIdx: 105, Velocity - 23.78 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6644
Frame 12: VelIdx: 109, Velocity - 26.10 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6644
Frame 12: VelIdx: 113, Velocity - 28.42 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6638
Frame 12: VelIdx: 117, Velocity - 30.74 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6644
Frame 12: VelIdx: 121, Velocity - 33.06 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6650
Frame 12: VelIdx: 125, Velocity - 35.38 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6647
Frame 12: VelIdx:  95, Velocity - 17.98 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 4096
Frame 12: VelIdx:  97, Velocity - 19.14 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6369
Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6360
Frame 12: VelIdx: 105, Velocity - 23.78 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6357
Frame 12: VelIdx: 109, Velocity - 26.10 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6353
Frame 12: VelIdx: 113, Velocity - 28.42 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6357
Frame 12: VelIdx: 117, Velocity - 30.74 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6373
Frame 12: VelIdx: 121, Velocity - 33.06 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6366
Frame 12: VelIdx: 125, Velocity - 35.38 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6363
Frame 12: VelIdx:  34, Velocity - 19.72 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 4849
Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 4318
Frame 12: VelIdx:  38, Velocity - 22.04 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 4937
Frame 12: VelIdx:  54, Velocity - 31.32 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 4811
Frame 12: VelIdx:  58, Velocity - 33.64 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 4886
Frame 12: VelIdx:  60, Velocity - 34.80 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 3713
Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 4026
Frame 12: VelIdx:  62, Velocity - 35.96 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 4811
Frame 12: VelIdx:  33, Velocity - 19.14 m/s, RangeIdx:  22, Range -  28.38 m, Energy - 5136
Frame 12: VelIdx:  35, Velocity - 20.30 m/s, RangeIdx:  22, Range -  28.38 m, Energy - 3965
Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  22, Range -  28.38 m, Energy - 5039
Frame 12: VelIdx:  41, Velocity - 23.78 m/s, RangeIdx:  22, Range -  28.38 m, Energy - 5077
Frame 12: VelIdx:  57, Velocity - 33.06 m/s, RangeIdx:  22, Range -  28.38 m, Energy - 5105
Frame 12: VelIdx:  59, Velocity - 34.22 m/s, RangeIdx:  22, Range -  28.38 m, Energy - 3845
Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  22, Range -  28.38 m, Energy - 5114
Frame 12: VelIdx:  63, Velocity - 36.54 m/s, RangeIdx:  22, Range -  28.38 m, Energy - 3873
Frame 12: VelIdx:  96, Velocity - 18.56 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 4439
Frame 12: VelIdx:  97, Velocity - 19.14 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 4129
Frame 12: VelIdx:  98, Velocity - 19.72 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 5036
Frame 12: VelIdx: 100, Velocity - 20.88 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 4456
Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 4757
Frame 12: VelIdx: 102, Velocity - 22.04 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 5043
Frame 12: VelIdx:  97, Velocity - 19.14 m/s, RangeIdx:  22, Range -  28.38 m, Energy - 5449
Frame 12: VelIdx:  99, Velocity - 20.30 m/s, RangeIdx:  22, Range -  28.38 m, Energy - 4257
Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  22, Range -  28.38 m, Energy - 5367

  • Hi Yao,

       Please find my answers inlined :

    1. We compared the RDM directly output from TI board and the RDM generated by applying  2D-FFT to raw ADC data divided by 16, and found that the elements of the former is much less than the latter. Could you elaborate on how  RDM is generated by TI? Is  the value of RDM elements in log2 domain?

    >>> The output of 2D FFT is not in log domain. What is the FFT dimension for range and doppler which you are using. Also what is the input data range? 

    2. In the CFAR  detection list ouptut from TI board, there are indices of Doppler and range bins and the associated energy (see attachment). I used the indices of the detected bins and found that the energy is quite different from that shown in detection list. How is the energy of the detection list calculated ?

    >>> Output energy of the peak detection applet is stored in binary log format thats why it could be very different from actual energy.

    3. How are the multiple channels combined to do CFAR? Noncoherently combining, i.e., log2(abs(rdm_0).^2+...+abs(rdm_N).^2)?

    >>> First we calculate the sum of energy across multiple channels ( not in log domain), this energy sum is in 32 bit. This is then coverted to 16 bit energy by using binary log.

    Regards,

    Anshu

  • Hi Anshu,

    The attached file target12.txt is detection list of CFAR. You can see the energy output is more than 2000. It looks like not log2 value.

    RadarMode - 1, NumOfDets - 1475
    Frame 12: VelIdx: 0, Velocity - 0.00 m/s, RangeIdx: 33, Range - 42.57 m, Energy - 2912
    Frame 12: VelIdx: 0, Velocity - 0.00 m/s, RangeIdx: 34, Range - 43.86 m, Energy - 3961
    Frame 12: VelIdx: 0, Velocity - 0.00 m/s, RangeIdx: 35, Range - 45.15 m, Energy - 4827

    ...

     

    The attached file RDM12_Rx0.txt is 2D FFT output. The rangeXDoppler dimension is 256X128. The amplitude of RDM varies from 0 to 384.9480.

     

    Thanks

    YaoRDM12_Rx0.txt

    RadarMode - 1, NumOfDets - 1475
    Frame 12: VelIdx:   0, Velocity -  0.00 m/s, RangeIdx:  33, Range -  42.57 m, Energy - 2912
    Frame 12: VelIdx:   0, Velocity -  0.00 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 3961
    Frame 12: VelIdx:   0, Velocity -  0.00 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 4827
    Frame 12: VelIdx:   0, Velocity -  0.00 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 5105
    Frame 12: VelIdx:   0, Velocity -  0.00 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 4824
    Frame 12: VelIdx:   0, Velocity -  0.00 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 3883
    Frame 12: VelIdx:   1, Velocity -  0.58 m/s, RangeIdx:  33, Range -  42.57 m, Energy - 2633
    Frame 12: VelIdx:   1, Velocity -  0.58 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 3671
    Frame 12: VelIdx:   1, Velocity -  0.58 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 4527
    Frame 12: VelIdx:   1, Velocity -  0.58 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 4808
    Frame 12: VelIdx:   1, Velocity -  0.58 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 4527
    Frame 12: VelIdx:   1, Velocity -  0.58 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 3589
    Frame 12: VelIdx:   2, Velocity -  1.16 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 2785
    Frame 12: VelIdx:   2, Velocity -  1.16 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 3632
    Frame 12: VelIdx:   2, Velocity -  1.16 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 3903
    Frame 12: VelIdx:   2, Velocity -  1.16 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 3627
    Frame 12: VelIdx:   2, Velocity -  1.16 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 2685
    Frame 12: VelIdx:   3, Velocity -  1.74 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 2121
    Frame 12: VelIdx:  33, Velocity - 19.14 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5136
    Frame 12: VelIdx:  33, Velocity - 19.14 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 6029
    Frame 12: VelIdx:  33, Velocity - 19.14 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6308
    Frame 12: VelIdx:  33, Velocity - 19.14 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6033
    Frame 12: VelIdx:  33, Velocity - 19.14 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 5136
    Frame 12: VelIdx:  34, Velocity - 19.72 m/s, RangeIdx:  33, Range -  42.57 m, Energy - 4849
    Frame 12: VelIdx:  34, Velocity - 19.72 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5419
    Frame 12: VelIdx:  34, Velocity - 19.72 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 5444
    Frame 12: VelIdx:  34, Velocity - 19.72 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 4989
    Frame 12: VelIdx:  34, Velocity - 19.72 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 4107
    Frame 12: VelIdx:  35, Velocity - 20.30 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 3965
    Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  33, Range -  42.57 m, Energy - 4318
    Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5216
    Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 6033
    Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6305
    Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6017
    Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 5039
    Frame 12: VelIdx:  38, Velocity - 22.04 m/s, RangeIdx:  33, Range -  42.57 m, Energy - 4937
    Frame 12: VelIdx:  38, Velocity - 22.04 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5434
    Frame 12: VelIdx:  38, Velocity - 22.04 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 5444
    Frame 12: VelIdx:  38, Velocity - 22.04 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 4960
    Frame 12: VelIdx:  41, Velocity - 23.78 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 6037
    Frame 12: VelIdx:  41, Velocity - 23.78 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6305
    Frame 12: VelIdx:  41, Velocity - 23.78 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6022
    Frame 12: VelIdx:  41, Velocity - 23.78 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 5077
    Frame 12: VelIdx:  45, Velocity - 26.10 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6308
    Frame 12: VelIdx:  49, Velocity - 28.42 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6308
    Frame 12: VelIdx:  53, Velocity - 30.74 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 6013
    Frame 12: VelIdx:  53, Velocity - 30.74 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6301
    Frame 12: VelIdx:  53, Velocity - 30.74 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6033
    Frame 12: VelIdx:  54, Velocity - 31.32 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5424
    Frame 12: VelIdx:  54, Velocity - 31.32 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 5458
    Frame 12: VelIdx:  57, Velocity - 33.06 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5188
    Frame 12: VelIdx:  57, Velocity - 33.06 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 6041
    Frame 12: VelIdx:  57, Velocity - 33.06 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6308
    Frame 12: VelIdx:  57, Velocity - 33.06 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6029
    Frame 12: VelIdx:  57, Velocity - 33.06 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 5105
    Frame 12: VelIdx:  58, Velocity - 33.64 m/s, RangeIdx:  33, Range -  42.57 m, Energy - 4886
    Frame 12: VelIdx:  58, Velocity - 33.64 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5429
    Frame 12: VelIdx:  58, Velocity - 33.64 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 5434
    Frame 12: VelIdx:  58, Velocity - 33.64 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 4946
    Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  33, Range -  42.57 m, Energy - 4026
    Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5178
    Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 6033
    Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6308
    Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6033
    Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 5114
    Frame 12: VelIdx:  62, Velocity - 35.96 m/s, RangeIdx:  33, Range -  42.57 m, Energy - 4811
    Frame 12: VelIdx:  62, Velocity - 35.96 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5392
    Frame 12: VelIdx:  62, Velocity - 35.96 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 5429
    Frame 12: VelIdx:  62, Velocity - 35.96 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 4977
    Frame 12: VelIdx:  63, Velocity - 36.54 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 3873
    Frame 12: VelIdx:  33, Velocity - 19.14 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5136
    Frame 12: VelIdx:  33, Velocity - 19.14 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 6029
    Frame 12: VelIdx:  33, Velocity - 19.14 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6308
    Frame 12: VelIdx:  34, Velocity - 19.72 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5419
    Frame 12: VelIdx:  34, Velocity - 19.72 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 5444
    Frame 12: VelIdx:  34, Velocity - 19.72 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 4989
    Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5216
    Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 6033
    Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6305
    Frame 12: VelIdx:  38, Velocity - 22.04 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5434
    Frame 12: VelIdx:  38, Velocity - 22.04 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 5444
    Frame 12: VelIdx:  38, Velocity - 22.04 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 4960
    Frame 12: VelIdx:  41, Velocity - 23.78 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5220
    Frame 12: VelIdx:  41, Velocity - 23.78 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 6037
    Frame 12: VelIdx:  41, Velocity - 23.78 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6305
    Frame 12: VelIdx:  45, Velocity - 26.10 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6308
    Frame 12: VelIdx:  49, Velocity - 28.42 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6308
    Frame 12: VelIdx:  53, Velocity - 30.74 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 6013
    Frame 12: VelIdx:  53, Velocity - 30.74 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6301
    Frame 12: VelIdx:  54, Velocity - 31.32 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5424
    Frame 12: VelIdx:  54, Velocity - 31.32 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 5458
    Frame 12: VelIdx:  57, Velocity - 33.06 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5188
    Frame 12: VelIdx:  57, Velocity - 33.06 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 6041
    Frame 12: VelIdx:  57, Velocity - 33.06 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6308
    Frame 12: VelIdx:  58, Velocity - 33.64 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5429
    Frame 12: VelIdx:  58, Velocity - 33.64 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 5434
    Frame 12: VelIdx:  58, Velocity - 33.64 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 4946
    Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5178
    Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 6033
    Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6308
    Frame 12: VelIdx:  62, Velocity - 35.96 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5392
    Frame 12: VelIdx:  62, Velocity - 35.96 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 5429
    Frame 12: VelIdx:  62, Velocity - 35.96 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 4977
    Frame 12: VelIdx:  33, Velocity - 19.14 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6033
    Frame 12: VelIdx:  34, Velocity - 19.72 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 4107
    Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6017
    Frame 12: VelIdx:  41, Velocity - 23.78 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6022
    Frame 12: VelIdx:  53, Velocity - 30.74 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6033
    Frame 12: VelIdx:  57, Velocity - 33.06 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6029
    Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6033
    Frame 12: VelIdx:  62, Velocity - 35.96 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 3974
    Frame 12: VelIdx:  97, Velocity - 19.14 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5467
    Frame 12: VelIdx:  97, Velocity - 19.14 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 6363
    Frame 12: VelIdx:  97, Velocity - 19.14 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6647
    Frame 12: VelIdx:  97, Velocity - 19.14 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6369
    Frame 12: VelIdx:  97, Velocity - 19.14 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 5449
    Frame 12: VelIdx:  98, Velocity - 19.72 m/s, RangeIdx:  33, Range -  42.57 m, Energy - 5036
    Frame 12: VelIdx:  98, Velocity - 19.72 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5626
    Frame 12: VelIdx:  98, Velocity - 19.72 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 5643
    Frame 12: VelIdx:  98, Velocity - 19.72 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 5089
    Frame 12: VelIdx:  99, Velocity - 20.30 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 4257
    Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  33, Range -  42.57 m, Energy - 4757
    Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5558
    Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 6373
    Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6644
    Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6360
    Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 5367
    Frame 12: VelIdx: 102, Velocity - 22.04 m/s, RangeIdx:  33, Range -  42.57 m, Energy - 5043
    Frame 12: VelIdx: 102, Velocity - 22.04 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5620
    Frame 12: VelIdx: 102, Velocity - 22.04 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 5626
    Frame 12: VelIdx: 102, Velocity - 22.04 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 5013
    Frame 12: VelIdx: 105, Velocity - 23.78 m/s, RangeIdx:  34, Range -  43.86 m, Energy - 5544
    Frame 12: VelIdx: 105, Velocity - 23.78 m/s, RangeIdx:  35, Range -  45.15 m, Energy - 6369
    Frame 12: VelIdx: 105, Velocity - 23.78 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6644
    Frame 12: VelIdx: 105, Velocity - 23.78 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6357
    Frame 12: VelIdx: 105, Velocity - 23.78 m/s, RangeIdx:  38, Range -  49.02 m, Energy - 5364
    Frame 12: VelIdx: 109, Velocity - 26.10 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6644
    Frame 12: VelIdx: 109, Velocity - 26.10 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6353
    Frame 12: VelIdx: 113, Velocity - 28.42 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6638
    Frame 12: VelIdx: 113, Velocity - 28.42 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6357
    Frame 12: VelIdx: 117, Velocity - 30.74 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6644
    Frame 12: VelIdx: 117, Velocity - 30.74 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6373
    Frame 12: VelIdx: 121, Velocity - 33.06 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6650
    Frame 12: VelIdx: 121, Velocity - 33.06 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6366
    Frame 12: VelIdx: 125, Velocity - 35.38 m/s, RangeIdx:  36, Range -  46.44 m, Energy - 6647
    Frame 12: VelIdx: 125, Velocity - 35.38 m/s, RangeIdx:  37, Range -  47.73 m, Energy - 6363
    Frame 12: VelIdx:  95, Velocity - 17.98 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 4385
    Frame 12: VelIdx:  97, Velocity - 19.14 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5467
    Frame 12: VelIdx:  97, Velocity - 19.14 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 6363
    Frame 12: VelIdx:  97, Velocity - 19.14 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6647
    Frame 12: VelIdx:  98, Velocity - 19.72 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5626
    Frame 12: VelIdx:  98, Velocity - 19.72 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 5643
    Frame 12: VelIdx:  98, Velocity - 19.72 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 5089
    Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5558
    Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 6373
    Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6644
    Frame 12: VelIdx: 102, Velocity - 22.04 m/s, RangeIdx:  18, Range -  23.22 m, Energy - 5620
    Frame 12: VelIdx: 102, Velocity - 22.04 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 5626
    Frame 12: VelIdx: 105, Velocity - 23.78 m/s, RangeIdx:  19, Range -  24.51 m, Energy - 6369
    Frame 12: VelIdx: 105, Velocity - 23.78 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6644
    Frame 12: VelIdx: 109, Velocity - 26.10 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6644
    Frame 12: VelIdx: 113, Velocity - 28.42 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6638
    Frame 12: VelIdx: 117, Velocity - 30.74 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6644
    Frame 12: VelIdx: 121, Velocity - 33.06 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6650
    Frame 12: VelIdx: 125, Velocity - 35.38 m/s, RangeIdx:  20, Range -  25.80 m, Energy - 6647
    Frame 12: VelIdx:  95, Velocity - 17.98 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 4096
    Frame 12: VelIdx:  97, Velocity - 19.14 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6369
    Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6360
    Frame 12: VelIdx: 105, Velocity - 23.78 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6357
    Frame 12: VelIdx: 109, Velocity - 26.10 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6353
    Frame 12: VelIdx: 113, Velocity - 28.42 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6357
    Frame 12: VelIdx: 117, Velocity - 30.74 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6373
    Frame 12: VelIdx: 121, Velocity - 33.06 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6366
    Frame 12: VelIdx: 125, Velocity - 35.38 m/s, RangeIdx:  21, Range -  27.09 m, Energy - 6363
    Frame 12: VelIdx:  34, Velocity - 19.72 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 4849
    Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 4318
    Frame 12: VelIdx:  38, Velocity - 22.04 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 4937
    Frame 12: VelIdx:  54, Velocity - 31.32 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 4811
    Frame 12: VelIdx:  58, Velocity - 33.64 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 4886
    Frame 12: VelIdx:  60, Velocity - 34.80 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 3713
    Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 4026
    Frame 12: VelIdx:  62, Velocity - 35.96 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 4811
    Frame 12: VelIdx:  33, Velocity - 19.14 m/s, RangeIdx:  22, Range -  28.38 m, Energy - 5136
    Frame 12: VelIdx:  35, Velocity - 20.30 m/s, RangeIdx:  22, Range -  28.38 m, Energy - 3965
    Frame 12: VelIdx:  37, Velocity - 21.46 m/s, RangeIdx:  22, Range -  28.38 m, Energy - 5039
    Frame 12: VelIdx:  41, Velocity - 23.78 m/s, RangeIdx:  22, Range -  28.38 m, Energy - 5077
    Frame 12: VelIdx:  57, Velocity - 33.06 m/s, RangeIdx:  22, Range -  28.38 m, Energy - 5105
    Frame 12: VelIdx:  59, Velocity - 34.22 m/s, RangeIdx:  22, Range -  28.38 m, Energy - 3845
    Frame 12: VelIdx:  61, Velocity - 35.38 m/s, RangeIdx:  22, Range -  28.38 m, Energy - 5114
    Frame 12: VelIdx:  63, Velocity - 36.54 m/s, RangeIdx:  22, Range -  28.38 m, Energy - 3873
    Frame 12: VelIdx:  96, Velocity - 18.56 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 4439
    Frame 12: VelIdx:  97, Velocity - 19.14 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 4129
    Frame 12: VelIdx:  98, Velocity - 19.72 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 5036
    Frame 12: VelIdx: 100, Velocity - 20.88 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 4456
    Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 4757
    Frame 12: VelIdx: 102, Velocity - 22.04 m/s, RangeIdx:  17, Range -  21.93 m, Energy - 5043
    Frame 12: VelIdx:  97, Velocity - 19.14 m/s, RangeIdx:  22, Range -  28.38 m, Energy - 5449
    Frame 12: VelIdx:  99, Velocity - 20.30 m/s, RangeIdx:  22, Range -  28.38 m, Energy - 4257
    Frame 12: VelIdx: 101, Velocity - 21.46 m/s, RangeIdx:  22, Range -  28.38 m, Energy - 5367
    

  • Hi,

       Can you refer peak_detection_cn function to see the processing which is happening for peak detection. You can find this function in peak_detection_tb.c file which is located at apps\peak_detection\test\src. Following is the function which is converting 32 bit energies to 16 bit energy :vcop_peak_detection_binlog_energy_scaling_cn

    Regards,

    Anshu

  • Hi,

      Another point which I forgot to add is that as EVE is a fixed point processor the energy is stored in a Q format, that is why it could be large. You can refer PEAK_DETECTION_TB_LUT_Q_FORMAT ( 8)  to see the Q format used for the energy

    Regards,

    Anshu