Part Number: PROCESSOR-SDK-AM65X
Tool/software: TI C/C++ Compiler
Hi:
We found the following U-disk recognition problem in using EVM boards under u-boot.
Test environment:
Hardware: AM654X EVM PROCESSOR BOARD (REV 1.0), 8G miscro SD card (Panasonic)
USB-HUB (Standard Microsystems, Realtek Semiconductor, Ithink)
U-disk (Sandisk , Kingston , HP ,Sansumg ,BANQ )
Software: Processor SDK Linux 06_00_00_07
Detailed description of the problem:
In U-boot, the EVM board connects a certain type of USB HUB and inserts the U disk, some of which can not be recognized.
The test topology is as follows. The EVM board has tested three different manufacturers'USB-HUB.
The first and second types of USB-HUB can be recognized normally, while the third type of USB-HUB(Standard microsystems chip: USB2514) has two types of USB-HUB that can not be recognized.But these two U disks can be correctly identified under Linux. The two U disks are BANQ (F30/64G) and Sandisk (SDCZ33/32G).