I have a custom built board running Linux with DVSDK. I have successfully created a Codec Engine DSP server and have a few questions.
The Codec Engine DSP server that contains several algorithms that need to be called from an Linux application that never ends. I have a couple of questions.
1. Should I open and close the handle to the engine for each Algorithm or should I open the Codec Engine and never close it?
Currently my application is built in Linux with no DSP algorithms.
1. Should I add the algorithm create, process, and control functions to my existing Linux application and then build it with the necessary DSP tools?
2. Or should each algorithm be a separate application that my current application calls into somehow? ?
Hopefully someone can give me some tips.
Thanks.