This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5728: DSP interrupt issue

Part Number: AM5728

Tool/software: Linux

Hello,

The experiment environment:

  • AM5728 IDK Board
  • ti-processor_sdk_rtos_am57xx_4_03_00_05 and CSL ePWM examples for C66 and M4
  • PROCESSOR-SDK-LINUX-RT-AM57X for A15

The experiment step:

  1. Boot the board and stop at UBoot
  2. Release C66 and load code of ePWM (attached in the end)
  3. Use UBoot command to
    1. enable epwm interrupt
    2. wait for 10 sec
    3. disable epwm interrupt
  4. Check the value of the counter, which is 0x40301000, to get the numbers of the ePWM interrupt handled by C66x.

The following figure has shown C66x cannot deal with 16Khz interrupts from ePWM. However, it seems easy for M4 to deal with 50Khz interrupt from ePWM. I have put everything (code, data, stack, ..) into internal SRAM to make C66x as busy as possible. Could someone provide any comment?

/*
 *  Copyright (c) Texas Instruments Incorporated 2017
 *
 *  Redistribution and use in source and binary forms, with or without
 *  modification, are permitted provided that the following conditions
 *  are met:
 *
 *    Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 *    Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the
 *    distribution.
 *
 *    Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
 *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
 *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
 *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
 *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
 *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
 *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
 *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
 *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
 *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
 *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 *
 */

/**
 *  \file     epwm_app.c
 *
 *  \brief    This file contains PWM test application which sets a particular
 *            duty cycle in PWMSS1 output A (EHRPWM1A) which can be verified
 *            through external pin probing.
 */

/* ========================================================================== */
/*                             Include Files                                  */
/* ========================================================================== */

#include "epwm_app.h"

/* ========================================================================== */
/*                                Macros                                      */
/* ========================================================================== */

/*
 * Configurable parameters
 */
/**
 *  \brief PWM instance base address.
 *
 *  Note: If changed to other instance, PRCM and pinmux changes needs to be
 *  taken care in the application.
 */
#define APP_EHRPWM_INST_BASE_ADDR       (SOC_PWMSS1_IPWMSS_BASE)

/**
 *  \brief Output channel - A or B.
 *
 *  Note: If changed to channel B, pinmux changes needs to be taken care
 *  in the application.
 */
#define APP_EHRPWM_OUTPUT_CH            (CSL_EPWM_OUTPUT_CH_A)

/** \brief Frequency of PWM output signal in Hz - 1 KHz is selected */
#define APP_EHRPWM_OUT_FREQ             50000 //(1U * 1000U)

/** \brief Duty Cycle of PWM output signal in % - give value from 0 to 100 */
#define APP_EHRPWM_DUTY_CYCLE           (25U)

/** \brief APP run time in seconds */
#define APP_RUN_TIME                    (10U)

/** \brief APP run count in event equal zero ISR count */
#define APP_RUN_TIME_ISRCOUNT           (APP_RUN_TIME * APP_EHRPWM_OUT_FREQ)

/**
 *  \brief Functional clock to the PWMSS.
 *  Fixed for the platform - can't be changed.
 */
#define SOC_EHRPWM_MODULE_FREQ          (133U * 1000U * 1000U)

/** \brief TB frequency in Hz - so that /4 divider is used */
#define APP_EHRPWM_TB_FREQ              (SOC_EHRPWM_MODULE_FREQ / 4U)

/**
 *  \brief PRD value - this determines the period
 *
 *  PRD = (TBCLK/PWM FREQ) / 2
 *  NOTE: /2 is added becasue up&down counter is selected. So period is 2 times
 */
#define APP_EHRPWM_PRD_VAL              ((APP_EHRPWM_TB_FREQ                   \
                                            / APP_EHRPWM_OUT_FREQ) / 2U)
/**
 *  \brief COMPA value - this determines the duty cycle
 *
 *  COMPA = (PRD - ((dutycycle * PRD) / 100)
 */
#define APP_EHRPWM_COMPA_VAL            (APP_EHRPWM_PRD_VAL -                  \
                                            ((APP_EHRPWM_DUTY_CYCLE *          \
                                                APP_EHRPWM_PRD_VAL) / 100U))

/*
#define APP_EHRPWM_INT                  (32U)
#define APP_EHRPWM_XBAR_CPU             (CSL_XBAR_IRQ_CPU_ID_IPU1)
#define APP_EHRPWM_XBAR_INST            (CSL_XBAR_INST_IPU1_IRQ_32)
#define APP_EHRPWM_XBAR_INTR_SOURCE     (CSL_XBAR_PWMSS1_IRQ_ePWM0INT)
*/

#define APP_EHRPWM_INT                  (32U)
#define APP_EHRPWM_XBAR_CPU             (CSL_XBAR_IRQ_CPU_ID_DSP1)
#define APP_EHRPWM_XBAR_INST            (CSL_XBAR_INST_DSP1_IRQ_32)
#define APP_EHRPWM_XBAR_INTR_SOURCE     (CSL_XBAR_PWMSS1_IRQ_ePWM0INT)
 

/* ========================================================================== */
/*                            Global Variables                                */
/* ========================================================================== */

/** \brief IP default configuration */
static CSL_EpwmAppPwmObj_t gAppPwmObj =
{
    APP_EHRPWM_OUTPUT_CH,                       /* pwmCh */
    APP_EHRPWM_INST_BASE_ADDR,                  /* instAddr */
    SOC_EHRPWM_MODULE_FREQ,                     /* funcClk */
    FALSE,                                      /* enableDeadband */
    FALSE,                                      /* enableChopper */
    FALSE,                                      /* enableTripzone */
    TRUE,                                       /* enableEventTrigger */
    FALSE,                                      /* enableHighResolution */
    /* CSL_EpwmAppPwmCfg_t*/
    {
        /* CSL_EpwmTimebaseCfg_t */
        {
            APP_EHRPWM_TB_FREQ,                 /* tbClk */
            APP_EHRPWM_OUT_FREQ,                /* pwmtbCounterFreqPrd */
            CSL_EPWM_TB_COUNTER_DIR_UP_DOWN,    /* tbCntrDirection */
            FALSE,                              /* enableSynchronization */
            PWMSS_EPWM_TBCTL_PHSDIR_COUNT_DOWN, /* cntDirAfterSync */
            0U,                                 /* phsCountAfterSync */
            PWMSS_EPWM_TBCTL_SYNCOSEL_EPWMXSYNC /* syncOutSrc */
        },
        /* CSL_EpwmCounterCmpCfg_t */
        {
            APP_EHRPWM_COMPA_VAL,               /* cmpAValue */
            APP_EHRPWM_COMPA_VAL                /* cmpBValue */
        },
        /* CSL_EpwmAqActionCfg_t */
        {
            CSL_EPWM_AQ_ACTION_DONOTHING,       /* zeroAction */
            CSL_EPWM_AQ_ACTION_DONOTHING,       /* prdAction */
            CSL_EPWM_AQ_ACTION_HIGH,            /* cmpAUpAction */
            CSL_EPWM_AQ_ACTION_LOW,             /* cmpADownAction */
            CSL_EPWM_AQ_ACTION_HIGH,            /* cmpBUpAction */
            CSL_EPWM_AQ_ACTION_LOW              /* cmpBDownAction */
        },
        /* CSL_EpwmDeadbandCfg_t */
        {
            CSL_EPWM_DB_IN_MODE_A_RED_A_FED,    /* inputMode */
            CSL_EPWM_DB_OUT_MODE_BYPASS,        /* outputMode */
            CSL_EPWM_DB_POL_SEL_ACTV_HIGH,      /* polaritySelect */
            0U,                                 /* risingEdgeDelay */
            0U                                  /* fallingEdgeDelay */
        },
        /* CSL_EpwmChopperCfg_t */
        {
            CSL_EPWM_CHP_DUTY_CYCLE_PERC_12PNT5,    /* dutyCycle */
            CSL_EPWM_CHP_CLK_FREQ_DIV_BY_1,         /* clkFrequency */
            CSL_EPWM_CHP_OSHT_WIDTH_1XSYSOUT_BY_8   /* oneShotPulseWidth */
        },
        /* CSL_EpwmTripzoneCfg_t */
        {
            CSL_EPWM_TZ_TRIP_ACTION_DO_NOTHING, /* tripAction */
            CSL_EPWM_TZ_EVENT_ONE_SHOT,         /* tripEvtType */
            0U,                                 /* tripPin */
            FALSE                               /* enableTripIntr */
        },
        /* CSL_EpwmEtCfg_t */
        {
            CSL_EPWM_ET_INTR_EVT_CNT_EQ_ZRO,    /* intrEvtSource */
            CSL_EPWM_ET_INTR_PERIOD_FIRST_EVT   /* intrPrd */
        }
    }
};

static volatile uint32_t gNumIsr = 0U;
volatile uint32_t *gNumIsr2 = (volatile uint32_t*)0x40301000;

#if defined (SOC_TDA2XX) || defined (SOC_TDA2PX) || defined (SOC_DRA75x) || defined (SOC_TDA2EX) || defined (SOC_DRA72x)
static uint32_t uartBaseAddr = SOC_UART1_BASE;
#endif
#if defined (SOC_TDA3XX) || defined (SOC_DRA78x)
static uint32_t uartBaseAddr = SOC_UART3_BASE;
#endif
static uint32_t uartBaseAddr = SOC_UART3_BASE;

/* ========================================================================== */
/*                 Internal Function Declarations                             */
/* ========================================================================== */

static void AppPwmIntrISR(void *handle);

static void CSL_epwmAppPwmCfg(CSL_EpwmAppPwmObj_t *pObj);
static void EpwmAppTimebaseModuleCfg(uint32_t baseAddr,
                                     uint32_t pwmFuncClk,
                                     CSL_EpwmTimebaseCfg_t *pTbCfg);
static void EpwmAppCounterComparatorCfg(uint32_t baseAddr,
                                        CSL_EpwmCounterCmpCfg_t *pCcCfg);

static void padConfig_prcmEnable(void);

/* ========================================================================== */
/*                          Function Definitions                              */
/* ========================================================================== */

int32_t main(void)
{
    CSL_EpwmAppPwmObj_t *pObj = &gAppPwmObj;

    /* Do pad config amd PRCM enable for UART and PWM */
    padConfig_prcmEnable();

    /* Initialize the UART Instance */
    UARTConfigInit(uartBaseAddr, BAUD_RATE_115200,
                   UART_WORD_LENGTH_8, UART_STOP_BIT_1,
                   UART_NO_PARITY, UART_16x_MODE);
    UARTConfigPuts(uartBaseAddr,
        "\nStarting EPWM duty cycle test application...\n", -1);
    UARTConfigPuts(
        uartBaseAddr, "Probe the PWM signal to verify...\n"
        "App will wait for 10 seconds (using  PWM period ISR)...\n", -1);
    UARTConfigPuts(uartBaseAddr,
        "Probe "
#if defined (SOC_TDA2XX) || defined (SOC_TDA2PX) || defined (SOC_DRA75x) || defined (SOC_TDA2EX) || defined (SOC_DRA72x)
        "VIN2A_VSYNC0 pin (RU19 pin 12) "
#endif
#if defined (SOC_TDA3XX) || defined (SOC_DRA78x)
        "GPMC_BEN0 pin (R9017/M1 of VISU connector) "
#endif
        "for 1KHz @ 25% duty cycle waveform...\n", -1);

    /* Enable clocks for EPWM module inside the PWM sub system. */
    CSL_epwmClockEnable(pObj->instAddr);

    /* EPWM channel configuration */
    CSL_epwmAppPwmCfg(pObj);

    *gNumIsr2 = 0;

    /* Wait for ISR count */
    //while (gNumIsr < APP_RUN_TIME_ISRCOUNT);
    while(1);

    //UARTConfigPuts(uartBaseAddr, "\nApplication is completed!!\n", -1);
    //return 0;
}

static void AppPwmIntrISR(void *handle)
{
    uint16_t status = CSL_epwmEtIntrStatus(APP_EHRPWM_INST_BASE_ADDR);

    CSL_epwmEtIntrClear(APP_EHRPWM_INST_BASE_ADDR);
    //gNumIsr++;
    *gNumIsr2 = (*gNumIsr2) + 1;
    return;
}

/**
 * \brief   This API configures the ePWM module
 *
 * \param   pObj             pointer to the ePwm object data structure.
 */
static void CSL_epwmAppPwmCfg(CSL_EpwmAppPwmObj_t *pObj)
{
    uint32_t baseAddr = pObj->instAddr;
    uint32_t pwmCh    = pObj->pwmCh;
    uint32_t pwmFuncClk = pObj->funcClk;
    CSL_EpwmAppPwmCfg_t *pPwmCfg = &pObj->pwmCfg;

    /* Configure the Time base Sub-Module */
    EpwmAppTimebaseModuleCfg(baseAddr, pwmFuncClk, &pPwmCfg->tbCfg);

    /* Counter-Comparator Sub-Module Configuration */
    EpwmAppCounterComparatorCfg(baseAddr, &pPwmCfg->ccCfg);

    /* Configure Action Qualifier */
    CSL_epwmAqActionOnOutputCfg(baseAddr, pwmCh, &pPwmCfg->aqCfg);

    /* Dead band sub-module configuration */
    if (TRUE == pObj->enableDeadband)
    {
       /* Enable and configure dead band sub module */
       CSL_epwmDeadbandCfg(baseAddr, &pPwmCfg->dbCfg);
    }
    else
    {
        /* Bypass dead band sub module */
        CSL_epwmDeadbandBypass(baseAddr);
    }

    /* Chopper sub-module configuration */
    if (TRUE == pObj->enableChopper)
    {
        /* Configure chopper sub - module */
        CSL_epwmChopperCfg(baseAddr, &pPwmCfg->chpCfg);

        /* Enable Chopper */
        CSL_epwmChopperEnable(baseAddr, TRUE);
    }
    else
    {
        /* Disable Chopper */
        CSL_epwmChopperEnable(baseAddr, FALSE);
    }

    /* Trip Zone Sub-Module Configuration */
    if (TRUE == pObj->enableTripZone)
    {
        /* Configure the Trip action */
        CSL_epwmTzTriggerTripAction(
            baseAddr, CSL_EPWM_TZ_TRIP_ACTION_HIGH, pwmCh);

        /* Enable the Trip event */
        CSL_epwmTzTripEventEnable(
            baseAddr, pPwmCfg->tzCfg.tripEvtType, pPwmCfg->tzCfg.tripPin);
    }
    else
    {
        /* Disable trip zone event handling and ignore all trip zone events */
        CSL_epwmTzTripEventDisable(
            baseAddr, CSL_EPWM_TZ_EVENT_ONE_SHOT, pPwmCfg->tzCfg.tripPin);
        CSL_epwmTzTripEventDisable(
            baseAddr, CSL_EPWM_TZ_EVENT_CYCLE_BY_CYCLE, pPwmCfg->tzCfg.tripPin);
    }

    /* Event trigger sub - module configuration */
    if (TRUE == pObj->enableEventTrigger)
    {
        /* Configure the Event trigger processing */
        CSL_epwmEtIntrCfg(
            baseAddr, pPwmCfg->etCfg.intrEvtSource, pPwmCfg->etCfg.intrPrd);
        CSL_epwmEtIntrEnable(baseAddr);
    }
    else
    {
        /* Disable Event trigger interrupts */
        CSL_epwmEtIntrDisable(baseAddr);
    }

    /**
     * High resolution feature is supported only on PWM A channel. If channel
     * is A then proceed with High Resolution processing.
     */
    if (CSL_EPWM_OUTPUT_CH_A == pwmCh)
    {
        if (TRUE == pObj->enableHighResolution)
        {
            /* configure high resolution feature */
            CSL_epwmHighResolutionCfg(
                baseAddr,
                pPwmCfg->hrCfg.delayBusSelect,
                pPwmCfg->hrCfg.delayMode);

            if (CSL_EPWM_HR_DELAY_BUS_SEL_CMPAHR ==
               pPwmCfg->hrCfg.delayBusSelect)
            {
                /* Load comparator A High-resolution counter value */
                CSL_epwmHrLoadCmpAHrValue(
                    baseAddr,
                    pPwmCfg->hrCfg.cmpAHighResVal,
                    CSL_EPWM_HR_REG_ACT_LOAD_CNT_ZRO_PULSE);
            }
            else  /* CSL_EPWM_HR_DELAY_BUS_SEL_TBPHSHR */
            {
                /* Load Timebase phase high resolution value */
                CSL_epwmHrLoadTbPhaseHrValue(
                    baseAddr, pPwmCfg->hrCfg.tbPhaseHighResVal);
            }
        }
        else
        {
            /* Disable High Resolution Feature */
            CSL_epwmHighResolutionDisable(baseAddr);
        }
    }

    return;
}

/**
 * \brief   This API configures the Timebase Sub-module.
 *
 * \param   baseAddr        Base address of PWMSS instance used
 * \param   pwmFuncClk      PWM functional clock value in Hz
 * \param   pTbCfg          Pointer to the Time base sub-module configuration
 *                          data structure
 */
static void EpwmAppTimebaseModuleCfg(uint32_t baseAddr,
                                     uint32_t pwmFuncClk,
                                     CSL_EpwmTimebaseCfg_t *pTbCfg)
{
    /* Configure Time base clock */
    CSL_epwmTbTimebaseClkCfg(baseAddr, pTbCfg->tbClk, pwmFuncClk);

    /* Configure PWM time base counter frequency and direction */
    CSL_epwmTbPwmFreqCfg(
        baseAddr,
        pTbCfg->tbClk,
        pTbCfg->pwmtbCounterFreqPrd,
        pTbCfg->tbCntrDirection,
        CSL_EPWM_SHADOW_REG_CTRL_ENABLE);

    if (TRUE == pTbCfg->enableSynchronization)
    {
        /* Enable Synchronization */
        CSL_epwmTbSyncEnable(
            baseAddr, pTbCfg->phsCountAfterSync, pTbCfg->cntDirAfterSync);
    }
    else
    {
        /* Disable Synchronization */
        CSL_epwmTbSyncDisable(baseAddr);
    }

    /* Configure Sync out signal */
    CSL_epwmTbSetSyncOutMode(baseAddr, pTbCfg->syncOutSrc);

    /* Configure the emulation behaviour */
    CSL_epwmTbSetEmulationMode(baseAddr, EPWM_TB_EMU_MODE_FREE_RUN);

    return;
}

/**
 * \brief   This API configures the Counter-Comparator Sub-module.
 *
 * \param   baseAddr    Base address of PWMSS instance used
 * \param   pCcCfg      Pointer to the Counter-Comparator Sub-module
 *                      configuration data structure
 */
static void EpwmAppCounterComparatorCfg(uint32_t baseAddr,
                                        CSL_EpwmCounterCmpCfg_t *pCcCfg)
{
    /* Counter Comparator A configuration */
    CSL_epwmCounterComparatorCfg(
        baseAddr,
        CSL_EPWM_CC_CMP_A,
        pCcCfg->cmpAValue,
        CSL_EPWM_SHADOW_REG_CTRL_ENABLE,
        CSL_EPWM_CC_CMP_LOAD_MODE_CNT_EQ_ZERO,
        TRUE);

    /* Counter Comparator B configuration */
    CSL_epwmCounterComparatorCfg(
        baseAddr,
        CSL_EPWM_CC_CMP_B,
        pCcCfg->cmpBValue,
        CSL_EPWM_SHADOW_REG_CTRL_ENABLE,
        CSL_EPWM_CC_CMP_LOAD_MODE_CNT_EQ_ZERO,
        TRUE);

    return;
}

static void padConfig_prcmEnable(void)
{
#if defined (SOC_TDA2XX) || defined (SOC_TDA2PX) || defined (SOC_DRA75x) || defined (SOC_TDA2EX) || defined (SOC_DRA72x)
    /* UART Pad configurations */
    HW_WR_REG32(
        SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_UART1_RXD, 0x00040000);
    HW_WR_REG32(
        SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_UART1_TXD, 0x00000000);

    /* PWM Pad configurations - VIN2A_VSYNC0 -> EHRPWM1A */
    HW_WR_REG32(
        SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_VIN2A_VSYNC0, 0x0000000A);
#endif
#if defined (SOC_TDA3XX) || defined (SOC_DRA78x)
    /* UART Pad configurations */
    HW_WR_REG32(
        SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_SPI1_SCLK, 0x00040001);
    HW_WR_REG32(
        SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_SPI1_CS0, 0x00000001);

    /* PWM Pad configurations - GPMC_BEN0 -> EHRPWM1A */
    HW_WR_REG32(
        SOC_CORE_PAD_IO_REGISTERS_BASE+CTRL_CORE_PAD_IO_GPMC_BEN0, 0x00000004);
#endif

    /* Enable PRCM for PWMSS1 */
    HW_WR_REG32(SOC_L4PER_CM_CORE_BASE + CM_L4PER2_PWMSS1_CLKCTRL, 0x2);
    while ((HW_RD_REG32(SOC_L4PER_CM_CORE_BASE +
                        CM_L4PER2_PWMSS1_CLKCTRL) & (0x00030000)) != 0x0) ;
    /* Time base clock for PWMSS1 module */
    HW_WR_FIELD32(
        SOC_CTRL_MODULE_CORE_CORE_REGISTERS_BASE + CTRL_CORE_CONTROL_IO_2,
        CTRL_CORE_CONTROL_IO_2_PWMSS1_TBCLKEN,
        1);

    /* XBar configuration */
    CSL_xbarIrqConfigure(
        APP_EHRPWM_XBAR_CPU, APP_EHRPWM_XBAR_INST, APP_EHRPWM_XBAR_INTR_SOURCE);

    /* Enable periodic interrupts for PWM period */
    Intc_Init();
    Intc_IntEnable(APP_EHRPWM_INT);

    /* Register ISR */
    Intc_IntRegister(APP_EHRPWM_INT, (IntrFuncPtr) AppPwmIntrISR, 0);
    Intc_IntPrioritySet(APP_EHRPWM_INT, 1, 0);
    Intc_SystemEnable(APP_EHRPWM_INT);

    return;
}
-stack  0x1000                             /* SOFTWARE STACK SIZE           */
-heap   0x2000                             /* HEAP AREA SIZE                */

/* SPECIFY THE SYSTEM MEMORY MAP */

MEMORY
{
        RST_START:      org = 0x00800000  len = 0x0300
        IRAM_MEM:       org = 0x00800300  len = 0x7c00
        MMU_TLB:		ORIGIN = 0x4031C000  LENGTH = 0x000004000
		/*SBL will use 1 KB of space from address 0x80000000 for EVE */
        DDR3_A8:		org = 0x80000400 len = (0x0B000000 - 0x400)    /* 176 MB */
        DDR3_BOOT:      org = 0x8B000000 len = 0x00010000    /* 32 MB */
		DDR3_DSP:		org = 0x8B010000 len = 0x01FF0000    /* 32 MB */
		DDR3_M3VPSS:	org = 0x8D000000 len = 0x01000000    /* 16 MB */
		DDR3_M3VIDEO:	org = 0x8E000000 len = 0x01000000    /* 16 MB */
		DDR3_SR0:		org = 0x8F000000 len = 0x01000000    /* 16 MB */
}

/* SPECIFY THE SECTIONS ALLOCATION INTO MEMORY */

SECTIONS
{
	boot :
	{
	 rts*.lib<boot.obj>(.text)
	}load > DDR3_BOOT

	.cachetest_ddrbuf > IRAM_MEM
    GROUP: load > IRAM_MEM
    {
        .bss:       /* UNINITIALIZED OR ZERO INITIALIZED */
        .neardata:
        .rodata:
    }
    BOARD_IO_DELAY_DATA : load > IRAM_MEM
    BOARD_IO_DELAY_CODE : load > IRAM_MEM
    .csl_vect : load > RST_START
    .vects : load > IRAM_MEM
    .l2_int  : load > IRAM_MEM
    .pmIdleFunc : load > IRAM_MEM
    .init    : load > IRAM_MEM
    .cio     : load > IRAM_MEM

    .text 	 : load > IRAM_MEM              /* CODE                         */
    .data    : load > IRAM_MEM              /* INITIALIZED GLOBAL AND STATIC VARIABLES. */
                                            /* GLOBAL & STATIC VARIABLES.   */
                    RUN_START(bss_start)
                    RUN_END(bss_end)
    .const   : load > IRAM_MEM              /* GLOBAL CONSTANTS             */
    .cinit   : load > IRAM_MEM
    .stack   : load > IRAM_MEM            /* SOFTWARE SYSTEM STACK        */
	.far	 : load > IRAM_MEM
	.plt     : load > IRAM_MEM
	.fardata : load > IRAM_MEM
	.switch	 : load > IRAM_MEM
	.my_sect_ddr : load > IRAM_MEM
	.sysmem : load > IRAM_MEM
}

  • Hi hungwei,

    Can you please try to add the ti\csl\arch\c66x\src\interrupt.c to your project and update the scanCombined() function to comment out the following for loop with the known interrupt number for PWM to see if it helps? The function takes about 18000 CPU cycles and is called twice in INTH_IRQHandler(). The INTH_IRQHandler() takes too much (about 40000 CPU cycles) EXCLUDING the 'inth_IrqHandler[intNumber[pass]](argArray[intNumber[pass]]);', i.e. AppPwmIntrISR() or TimerIsr() in another thread, which causes interrupt missed.

    DSP_INTC accepts up to 124 event inputs, and flexibly maps those down to 12 interrupt inputs to the DSP. The mapping uses the event combiner to map multiple interrupts (within a 32-bit group) to one of the DSP interrupt inputs. To determine the interrupt bit within the 32-bit group, scanCombined() is called.

    #if 0
    for (; i < 32U; i++)
    {
              if ((uint32_t) 0 != (flag & (uint32_t) ((uint32_t) 1U << i)))
             {
               intNo[count] = ((uint8_t) (i + (combNo << 5)));
                if (count < 31U)
                 {
                      count++;
                 }
              }
    }
    #end

    You will need to add something like below, please step into above for loop to confirm the intNo[ ] and 'count' number.
       intNo[0]=32;
        count = 1;

    Regards,
    Garrett

  • Hello Garrett,

    Thanks a lot. It seems work. 

    Regards,

    Hungwei