Part Number: AM4378
Tool/software: Linux
we are writing a program where we would like to have complete control of the backlight but it would appear that we do not.
linux SDK ti-processor-sdk-linux-am437x-evm-04.03.00.05
am4378 EVM
in the program, for right now weston is disabled at the start of the program via:
system("systemctl stop weston");
when the program is active and disabling the backlight off control in our code, if we don't touch anything for a while the backlight still turns off
is this a result of us not entirely disabling weston from start up or is something else controlling the backlight? if so how can i disable it so we are the only master?