Hi, This is LG electronics engineer.
I have a couple of question for PSDKRA_RTOS(v0.9).
Testing the CAN profile application within MCUSW of PSDKRA_RTOS(v0.9) in J721EXCP01EVM(Board).
1. In order to configure MCAL every configuration for testing this application, should I use the EB configurator ?
It is just one solution for configuring MCAL ?
If i should use the EB configurator, there is no installation guide which can follow in PSDKRA_RTOS(v0.9).
Also, this version's MCAL modules aren't delivered in the form of EBtresos plugins.
2. I see your every test report, you seem to just test "CAN example application" in csl folder through building and compiling the BAREMETAL type.
If i use the CAN example application, it is easy to execute this application through JTAG tool. However, because of some problem, we can't use JTAG.
We have to execute the CAN profile application in MCUSW.
In MCUSW, there is your test report. Is it tested through tirtos building version that some data is transmitted to external CANoe and received from CANoe through CAN communication ?
3. When i execute your CAN profile application, CANoe tool can't receive any data from your EVM. I was debugging it that can you give me a few advice such as using EB configurator etc. ?