Part Number: AM3352
Hi,
I'm asking this question on behalf of my customer.
"
I have question about GPIO drive ability, my project use am3352, have EMMC/SD/DDR3/dual-Ethernet and use most of pings.
I have 12 LEDs to indicate system status. drive current for each LED is about 3mA, I plan to use 12 GPIO to drive those 12 LEDs.
Is it OK for AM3352 to drive those 12 LEDs? Which is better: High (drive) or Low (sink) active?
"
My initial thoughts are that he should be fine with the amount of current since the maximum current that can be driven in each GPIO pin is 6mA, but I'm not sure whether high or low is better.
Thanks!
Lauren