Hi, I am using DM368 ipnc, when I set IP Address on UI and saving it ,
it will show "Network setting for failed for the camera TI_IPNC",
In fact, it has already modify in cfg file, I can use new IP address to login.
Port has the same error warning,
But when I change port from 80 to 8080, I can't use new port to login page,
it will show "Load App Error -5".
how can I solve this problem?