This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6548: Yocto build error

Part Number: AM6548

Hi ,

I am trying to build arago-base-tisdk-image for AM6548 .

Shell has been configured as dash.

i am getting the following error during build:

ERROR: input-utils-1.0-r0 do_configure: oe_runmake failed
ERROR: input-utils-1.0-r0 do_configure: Function failed: do_configure (log file is located at /home/shruthi/TI/tisdk/build/arago-tmp-external-arm-toolchain/work/aarch64-linux/input-utils/1.0-r0/temp/log.do_configure.30907)
ERROR: Logfile of failure stored in: /home/shruthi/TI/tisdk/build/arago-tmp-external-arm-toolchain/work/aarch64-linux/input-utils/1.0-r0/temp/log.do_configure.30907
Log data follows:
| DEBUG: Executing shell function do_configure
| NOTE: make DESTDIR=/home/shruthi/TI/tisdk/build/arago-tmp-external-arm-toolchain/work/aarch64-linux/input-utils/1.0-r0/image clean
| ERROR: oe_runmake failed
| Make.config:1: *** empty variable name. Stop.
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_configure (log file is located at /home/shruthi/TI/tisdk/build/arago-tmp-external-arm-toolchain/work/aarch64-linux/input-utils/1.0-r0/temp/log.do_configure.30907)