Part Number: AM3352
Other Parts Discussed in Thread: DP83620, DP83630, PCA9555, TUSB8041
Hi team, I using a LTE module through TUSB4041 connect to AM3352 USB1, when power on LTE module, Linux Kernel can correct enumerate every usb devices,dmesg as follow:
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.19.38 (test@test-virtual-machine) (gcc version 7.4.1 20181213 [linaro-7.4-2019.02 revision 56ec6f6b99cc167ff0c2f8e1a2eed33b1edc85d4] (Linaro GCC 7.4-2019.02)) #1 SMP PREEMPT Fri Aug 23 12:52:06 CST 2019
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: PDZ852-SENSOR
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] cma: Reserved 48 MiB at 0x8a800000
[ 0.000000] On node 0 totalpages: 65536
[ 0.000000] Normal zone: 576 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 65536 pages, LIFO batch:15
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (neon)
[ 0.000000] random: get_random_bytes called from start_kernel+0xa4/0x440 with crng_init=0
[ 0.000000] percpu: Embedded 15 pages/cpu s31756 r8192 d21492 u61440
[ 0.000000] pcpu-alloc: s31756 r8192 d21492 u61440 alloc=15*4096
[ 0.000000] pcpu-alloc: [0] 0
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 64960
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/nfs nfsroot=192.168.0.2:/home/test/rootfs/rootfs-dev,nolock rw ip=192.168.0.15:192.168.0.2:192.168.0.1:255.255.255.0::eth0:off
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 199428K/262144K available (7168K kernel code, 232K rwdata, 1844K rodata, 1024K init, 253K bss, 13564K reserved, 49152K cma-reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xd0800000 - 0xff800000 ( 752 MB)
lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
.text : 0x(ptrval) - 0x(ptrval) (8160 kB)
.init : 0x(ptrval) - 0x(ptrval) (1024 kB)
.data : 0x(ptrval) - 0x(ptrval) ( 233 kB)
.bss : 0x(ptrval) - 0x(ptrval) ( 254 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] IRQ: Found an INTC at 0x(ptrval) (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000021] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000051] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000068] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000316] timer_probe: no matching timers found
[ 0.000589] Console: colour dummy device 80x30
[ 0.000683] Calibrating delay loop... 597.60 BogoMIPS (lpj=2988032)
[ 0.118666] pid_max: default: 32768 minimum: 301
[ 0.118873] Security Framework initialized
[ 0.118896] Yama: becoming mindful.
[ 0.119026] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.119049] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.120301] CPU: Testing write buffer coherency: ok
[ 0.120396] CPU0: Spectre v2: using BPIALL workaround
[ 0.120971] CPU0: thread -1, cpu 0, socket -1, mpidr 0
[ 0.178771] Setting up static identity map for 0x80100000 - 0x80100060
[ 0.198663] rcu: Hierarchical SRCU implementation.
[ 0.238658] smp: Bringing up secondary CPUs ...
[ 0.238682] smp: Brought up 1 node, 1 CPU
[ 0.238698] SMP: Total of 1 processors activated (597.60 BogoMIPS).
[ 0.238711] CPU: All CPU(s) started in SVC mode.
[ 0.241021] devtmpfs: initialized
[ 0.258930] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.259576] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.259614] futex hash table entries: 256 (order: 2, 16384 bytes)
[ 0.264267] pinctrl core: initialized pinctrl subsystem
[ 0.266039] NET: Registered protocol family 16
[ 0.271938] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.301796] l4_wkup_cm:clk:0010:0: failed to disable
[ 0.357350] cpuidle: using governor ladder
[ 0.357422] cpuidle: using governor menu
[ 0.365237] gpio gpiochip0: (gpio-0-31): added GPIO chardev (254:0)
[ 0.365375] gpiochip_setup_dev: registered GPIOs 0 to 31 on device: gpiochip0 (gpio-0-31)
[ 0.365450] OMAP GPIO hardware version 0.1
[ 0.366369] gpio gpiochip1: Persistence not supported for GPIO 28
[ 0.366389] GPIO line 60 (ETHPHY_RESET_CTRL) hogged as output/high
[ 0.366694] gpio gpiochip1: (gpio-32-63): added GPIO chardev (254:1)
[ 0.366824] gpiochip_setup_dev: registered GPIOs 32 to 63 on device: gpiochip1 (gpio-32-63)
[ 0.367886] gpio gpiochip2: (gpio-64-95): added GPIO chardev (254:2)
[ 0.368006] gpiochip_setup_dev: registered GPIOs 64 to 95 on device: gpiochip2 (gpio-64-95)
[ 0.369281] gpio gpiochip3: (gpio-96-127): added GPIO chardev (254:3)
[ 0.369426] gpiochip_setup_dev: registered GPIOs 96 to 127 on device: gpiochip3 (gpio-96-127)
[ 0.382263] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.426940] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.427934] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/regulators/fixedregulator0[0]'
[ 0.428443] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/regulators/fixedregulator1[0]'
[ 0.429114] of_get_named_gpiod_flags: can't parse 'gpio' property of node '/regulators/fixedregulator2[0]'
[ 0.431426] media: Linux media interface: v0.10
[ 0.431505] videodev: Linux video capture interface: v2.00
[ 0.431568] pps_core: LinuxPPS API ver. 1 registered
[ 0.431582] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.431619] PTP clock support registered
[ 0.431673] EDAC MC: Ver: 3.0.0
[ 0.439539] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.441642] clocksource: Switched to clocksource timer1
[ 0.456523] NET: Registered protocol family 2
[ 0.457777] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes)
[ 0.457832] TCP established hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.457877] TCP bind hash table entries: 2048 (order: 2, 16384 bytes)
[ 0.457934] TCP: Hash tables configured (established 2048 bind 2048)
[ 0.458089] UDP hash table entries: 256 (order: 1, 8192 bytes)
[ 0.458129] UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
[ 0.458538] NET: Registered protocol family 1
[ 0.489718] RPC: Registered named UNIX socket transport module.
[ 0.489743] RPC: Registered udp transport module.
[ 0.489756] RPC: Registered tcp transport module.
[ 0.489768] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.491277] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.493553] Initialise system trusted keyrings
[ 0.494024] workingset: timestamp_bits=14 max_order=16 bucket_order=2
[ 0.502908] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.514091] NFS: Registering the id_resolver key type
[ 0.514154] Key type id_resolver registered
[ 0.514168] Key type id_legacy registered
[ 0.514238] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.514893] pstore: using deflate compression
[ 0.518316] Key type asymmetric registered
[ 0.518343] Asymmetric key parser 'x509' registered
[ 0.518448] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
[ 0.528837] io scheduler noop registered
[ 0.528860] io scheduler deadline registered
[ 0.529150] io scheduler cfq registered (default)
[ 0.529170] io scheduler mq-deadline registered
[ 0.529185] io scheduler kyber registered
[ 0.531980] pinctrl-single 44e10800.pinmux: 142 pins, size 568
[ 0.618717] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.624364] omap_uart 44e09000.serial: no wakeirq for uart0
[ 0.624435] of_get_named_gpiod_flags: can't parse 'rts-gpio' property of node '/ocp/serial@44e09000[0]'
[ 0.624476] 44e09000.serial: ttyO0 at MMIO 0x44e09000 (irq = 30, base_baud = 3000000) is a OMAP UART0
[ 1.305993] console [ttyO0] enabled
[ 1.310539] omap_uart 48022000.serial: no wakeirq for uart1
[ 1.316509] of_get_named_gpiod_flags: can't parse 'rts-gpio' property of node '/ocp/serial@48022000[0]'
[ 1.316671] 48022000.serial: ttyO1 at MMIO 0x48022000 (irq = 31, base_baud = 3000000) is a OMAP UART1
[ 1.327169] omap_uart 48024000.serial: no wakeirq for uart2
[ 1.333125] of_get_named_gpiod_flags: can't parse 'rts-gpio' property of node '/ocp/serial@48024000[0]'
[ 1.333245] 48024000.serial: ttyO2 at MMIO 0x48024000 (irq = 32, base_baud = 3000000) is a OMAP UART2
[ 1.343700] omap_uart 481a6000.serial: no wakeirq for uart3
[ 1.349587] of_get_named_gpiod_flags: can't parse 'rts-gpio' property of node '/ocp/serial@481a6000[0]'
[ 1.349704] 481a6000.serial: ttyO3 at MMIO 0x481a6000 (irq = 33, base_baud = 3000000) is a OMAP UART3
[ 1.360280] omap_uart 481a8000.serial: no wakeirq for uart4
[ 1.366304] of_get_named_gpiod_flags: can't parse 'rts-gpio' property of node '/ocp/serial@481a8000[0]'
[ 1.366422] 481a8000.serial: ttyO4 at MMIO 0x481a8000 (irq = 34, base_baud = 3000000) is a OMAP UART4
[ 1.376930] omap_uart 481aa000.serial: no wakeirq for uart5
[ 1.382881] of_get_named_gpiod_flags: can't parse 'rts-gpio' property of node '/ocp/serial@481aa000[0]'
[ 1.382998] 481aa000.serial: ttyO5 at MMIO 0x481aa000 (irq = 35, base_baud = 3000000) is a OMAP UART5
[ 1.394750] omap_rng 48310000.rng: Random Number Generator ver. 20
[ 1.417947] brd: module loaded
[ 1.434199] loop: module loaded
[ 1.441021] mdio_bus fixed-0: GPIO lookup for consumer reset
[ 1.441039] mdio_bus fixed-0: using lookup tables for GPIO lookup
[ 1.441052] mdio_bus fixed-0: No GPIO consumer reset found
[ 1.441095] libphy: Fixed MDIO Bus: probed
[ 1.461454] mdio_bus 4a101000.mdio: GPIO lookup for consumer reset
[ 1.461469] mdio_bus 4a101000.mdio: using device tree for GPIO lookup
[ 1.461503] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/ethernet@4a100000/mdio@4a101000[0]'
[ 1.461528] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp/ethernet@4a100000/mdio@4a101000[0]'
[ 1.461542] mdio_bus 4a101000.mdio: using lookup tables for GPIO lookup
[ 1.461554] mdio_bus 4a101000.mdio: No GPIO consumer reset found
[ 1.511718] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000
[ 1.519781] davinci_mdio 4a101000.mdio: detected phy mask fffffff5
[ 1.539089] libphy: 4a101000.mdio: probed
[ 1.543491] davinci_mdio 4a101000.mdio: phy[1]: device 4a101000.mdio:01, driver NatSemi DP83620/DP83630/83640 Without PTP
[ 1.555139] davinci_mdio 4a101000.mdio: phy[3]: device 4a101000.mdio:03, driver NatSemi DP83620/DP83630/83640 Without PTP
[ 1.567832] cpsw 4a100000.ethernet: Detected MACID = 0c:ae:7d:73:e0:9d
[ 1.575004] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
[ 1.581786] cpsw 4a100000.ethernet: ALE Table size 1024
[ 1.587324] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies)
[ 1.596601] cpsw 4a100000.ethernet: cpsw: Detected MACID = 0c:ae:7d:73:e0:9f
[ 1.606052] i2c /dev entries driver
[ 1.611537] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 1.619954] device-mapper: ioctl: 4.39.0-ioctl (2018-04-03) initialised: dm-devel@redhat.com
[ 1.641964] cpuidle: enable-method property 'ti,am3352' found operations
[ 1.649757] sdhci: Secure Digital Host Controller Interface driver
[ 1.656420] sdhci: Copyright(c) Pierre Ossman
[ 1.662047] omap_hsmmc 48060000.mmc: GPIO lookup for consumer cd
[ 1.662061] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 1.662121] of_get_named_gpiod_flags: parsed 'cd-gpios' property of node '/ocp/mmc@48060000[0]' - status (0)
[ 1.662225] gpio gpiochip0: Persistence not supported for GPIO 6
[ 1.662247] omap_gpio 44e07000.gpio: Could not set line 6 debounce to 200000 microseconds (-22)
[ 1.671396] omap_hsmmc 48060000.mmc: Got CD GPIO
[ 1.676330] omap_hsmmc 48060000.mmc: GPIO lookup for consumer wp
[ 1.676341] omap_hsmmc 48060000.mmc: using device tree for GPIO lookup
[ 1.676368] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@48060000[0]'
[ 1.676390] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@48060000[0]'
[ 1.676404] omap_hsmmc 48060000.mmc: using lookup tables for GPIO lookup
[ 1.676416] omap_hsmmc 48060000.mmc: No GPIO consumer wp found
[ 1.677024] omap_hsmmc 48060000.mmc: Linked as a consumer to regulator.1
[ 1.712192] omap_hsmmc 481d8000.mmc: GPIO lookup for consumer cd
[ 1.712221] omap_hsmmc 481d8000.mmc: using device tree for GPIO lookup
[ 1.712281] of_get_named_gpiod_flags: can't parse 'cd-gpios' property of node '/ocp/mmc@481d8000[0]'
[ 1.712325] of_get_named_gpiod_flags: can't parse 'cd-gpio' property of node '/ocp/mmc@481d8000[0]'
[ 1.712351] omap_hsmmc 481d8000.mmc: using lookup tables for GPIO lookup
[ 1.712374] omap_hsmmc 481d8000.mmc: No GPIO consumer cd found
[ 1.712401] omap_hsmmc 481d8000.mmc: GPIO lookup for consumer wp
[ 1.712420] omap_hsmmc 481d8000.mmc: using device tree for GPIO lookup
[ 1.712461] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@481d8000[0]'
[ 1.712501] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@481d8000[0]'
[ 1.712525] omap_hsmmc 481d8000.mmc: using lookup tables for GPIO lookup
[ 1.712545] omap_hsmmc 481d8000.mmc: No GPIO consumer wp found
[ 1.713636] omap_hsmmc 481d8000.mmc: Linked as a consumer to regulator.1
[ 1.745463] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.754388] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-sys/leds-sys0[0]' - status (0)
[ 1.754538] gpio gpiochip2: Persistence not supported for GPIO 4
[ 1.754553] no flags found for gpios
[ 1.754934] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-sys/leds-sys1[0]' - status (0)
[ 1.754974] gpio gpiochip2: Persistence not supported for GPIO 2
[ 1.754987] no flags found for gpios
[ 1.755892] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-user/led-user0[0]' - status (0)
[ 1.755999] gpio gpiochip3: Persistence not supported for GPIO 21
[ 1.756013] no flags found for gpios
[ 1.756363] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-user/led-user1[0]' - status (0)
[ 1.756402] gpio gpiochip2: Persistence not supported for GPIO 1
[ 1.756414] no flags found for gpios
[ 1.756706] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-user/led-user2[0]' - status (0)
[ 1.756744] gpio gpiochip3: Persistence not supported for GPIO 18
[ 1.756896] no flags found for gpios
[ 1.757326] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-user/led-user3[0]' - status (0)
[ 1.757369] gpio gpiochip0: Persistence not supported for GPIO 7
[ 1.757381] no flags found for gpios
[ 1.757826] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-user/led-user4[0]' - status (0)
[ 1.757867] gpio gpiochip1: Persistence not supported for GPIO 22
[ 1.757879] no flags found for gpios
[ 1.758297] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-user/led-user5[0]' - status (0)
[ 1.758337] gpio gpiochip1: Persistence not supported for GPIO 18
[ 1.758350] no flags found for gpios
[ 1.758773] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-user/led-user6[0]' - status (0)
[ 1.758813] gpio gpiochip1: Persistence not supported for GPIO 24
[ 1.758950] no flags found for gpios
[ 1.759380] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-user/led-user7[0]' - status (0)
[ 1.759419] gpio gpiochip0: Persistence not supported for GPIO 22
[ 1.759432] no flags found for gpios
[ 1.759854] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-user/led-user8[0]' - status (0)
[ 1.759892] gpio gpiochip0: Persistence not supported for GPIO 26
[ 1.759905] no flags found for gpios
[ 1.760351] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-user/led-user9[0]' - status (0)
[ 1.760390] gpio gpiochip1: Persistence not supported for GPIO 12
[ 1.760403] no flags found for gpios
[ 1.761362] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-iio/led-out0[0]' - status (0)
[ 1.761406] gpio gpiochip1: Persistence not supported for GPIO 17
[ 1.761418] no flags found for gpios
[ 1.761888] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-iio/led-out1[0]' - status (0)
[ 1.761931] gpio gpiochip1: Persistence not supported for GPIO 19
[ 1.761944] no flags found for gpios
[ 1.762368] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-iio/led-out2[0]' - status (0)
[ 1.762408] gpio gpiochip1: Persistence not supported for GPIO 23
[ 1.762421] no flags found for gpios
[ 1.762875] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-iio/led-out3[0]' - status (0)
[ 1.762915] gpio gpiochip2: Persistence not supported for GPIO 0
[ 1.762928] no flags found for gpios
[ 1.763229] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-iio/led-out4[0]' - status (0)
[ 1.763267] gpio gpiochip0: Persistence not supported for GPIO 30
[ 1.763280] no flags found for gpios
[ 1.765377] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.774271] sc1161y_probe() function is called.
[ 1.779088] of_get_named_gpiod_flags: parsed 'pwren-gpio' property of node '/ocp/spi@481a0000/encryption@0[0]' - status (0)
[ 1.779137] of_get_named_gpiod_flags: parsed 'ctrlcs-gpio' property of node '/ocp/spi@481a0000/encryption@0[0]' - status (0)
[ 1.779510] sc1161y encryption probe ok: got minor 63
[ 1.786654] NET: Registered protocol family 10
[ 1.804643] Segment Routing with IPv6
[ 1.808735] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 1.816604] NET: Registered protocol family 17
[ 1.821558] Key type dns_resolver registered
[ 1.826359] mmc1: new high speed MMC card at address 0001
[ 1.832374] Registering SWP/SWPB emulation handler
[ 1.837419] omap_voltage_late_init: Voltage driver support not added
[ 1.844147] random: fast init done
[ 1.849998] Loading compiled-in X.509 certificates
[ 1.859698] mmcblk1: mmc1:0001 IS004G 3.64 GiB
[ 1.872740] mmcblk1boot0: mmc1:0001 IS004G partition 1 2.00 MiB
[ 1.879750] mmcblk1boot1: mmc1:0001 IS004G partition 2 2.00 MiB
[ 1.894351] mmcblk1rpmb: mmc1:0001 IS004G partition 3 512 KiB, chardev (244:0)
[ 1.915311] mmcblk1: p1 p2 p3 p4
[ 1.933155] rtc rtc0: alarm rollover: day
[ 1.933867] rtc rtc0: rx8025: dev (252:0)
[ 1.933904] rtc-rx8025 0-0032: rtc core: registered rx8025 as rtc0
[ 1.940898] at24 0-0050: GPIO lookup for consumer wp
[ 1.940912] at24 0-0050: using device tree for GPIO lookup
[ 1.940948] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/i2c@44e0b000/baseboard_eeprom@50[0]'
[ 1.940973] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/i2c@44e0b000/baseboard_eeprom@50[0]'
[ 1.940988] at24 0-0050: using lookup tables for GPIO lookup
[ 1.941001] at24 0-0050: No GPIO consumer wp found
[ 1.941493] at24 0-0050: 4096 byte 24c32 EEPROM, writable, 1 bytes/write
[ 1.948791] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 1.956716] pca953x 1-0020: GPIO lookup for consumer reset
[ 1.956733] pca953x 1-0020: using device tree for GPIO lookup
[ 1.956766] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/i2c@4802a000/pca9555@20[0]'
[ 1.956788] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp/i2c@4802a000/pca9555@20[0]'
[ 1.956803] pca953x 1-0020: using lookup tables for GPIO lookup
[ 1.956814] pca953x 1-0020: No GPIO consumer reset found
[ 1.956986] pca953x 1-0020: Linked as a consumer to regulator.3
[ 1.993332] gpiochip_find_base: found new base at 496
[ 1.993682] gpio gpiochip4: (pca9555): added GPIO chardev (254:4)
[ 1.993824] gpiochip_setup_dev: registered GPIOs 496 to 511 on device: gpiochip4 (pca9555)
[ 1.993918] omap_i2c 4802a000.i2c: bus 1 rev0.11 at 100 kHz
[ 2.000485] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-iio/led-out0[0]' - status (0)
[ 2.000524] gpio gpiochip1: Persistence not supported for GPIO 17
[ 2.000531] no flags found for gpios
[ 2.000749] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-iio/led-out1[0]' - status (0)
[ 2.000771] gpio gpiochip1: Persistence not supported for GPIO 19
[ 2.000778] no flags found for gpios
[ 2.000957] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-iio/led-out2[0]' - status (0)
[ 2.000977] gpio gpiochip1: Persistence not supported for GPIO 23
[ 2.000984] no flags found for gpios
[ 2.001141] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-iio/led-out3[0]' - status (0)
[ 2.001163] gpio gpiochip2: Persistence not supported for GPIO 0
[ 2.001169] no flags found for gpios
[ 2.001323] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-iio/led-out4[0]' - status (0)
[ 2.001343] gpio gpiochip0: Persistence not supported for GPIO 30
[ 2.001350] no flags found for gpios
[ 2.001509] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-iio/led-out5[0]' - status (0)
[ 2.002417] no flags found for gpios
[ 2.003631] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-iio/led-out6[0]' - status (0)
[ 2.004241] no flags found for gpios
[ 2.005382] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-iio/led-out7[0]' - status (0)
[ 2.005997] no flags found for gpios
[ 2.007151] of_get_named_gpiod_flags: parsed 'gpios' property of node '/leds-iio/led-out8[0]' - status (0)
[ 2.007746] no flags found for gpios
[ 2.009549] rtc-rx8025 0-0032: Starting synchronization hwclcok to system clock
[ 2.017374] rtc-rx8025 0-0032: Synchronization ...
[ 3.073300] rtc-rx8025 0-0032: Complete synchronization hwclcok to system clock(15)
[ 3.081416] rtc-rx8025 0-0032: setting system clock to 2019-08-23 13:53:58 UTC (1566568438)
[ 3.090354] rtc-rx8025 0-0032: Read system clock:tv_sec=(1566568438), tv_usec=208972
[ 3.116124] net eth0: initializing cpsw version 1.12 (0)
[ 3.222138] NatSemi DP83620/DP83630/83640 Without PTP 4a101000.mdio:01: attached PHY driver [NatSemi DP83620/DP83630/83640 Without PTP] (mii_bus:phy_addr=4a101000.mdio:01, irq=POLL)
[ 3.246801] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 6.322855] cpsw 4a100000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 6.341842] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 6.371853] IP-Config: Complete:
[ 6.375268] device=eth0, hwaddr=0c:ae:7d:73:e0:9d, ipaddr=192.168.0.15, mask=255.255.255.0, gw=192.168.0.1
[ 6.386210] host=192.168.0.15, domain=, nis-domain=(none)
[ 6.392538] bootserver=192.168.0.2, rootserver=192.168.0.2, rootpath=
[ 6.429695] VFS: Mounted root (nfs filesystem) on device 0:14.
[ 6.437522] devtmpfs: mounted
[ 6.443808] Freeing unused kernel memory: 1024K
[ 6.449180] Run /sbin/init as init process
[ 7.933382] systemd[1]: systemd 237 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ +LZ4 +SECCOMP +BLKID +ELFUTILS +KMOD -IDN2 +IDN -PCRE2 default-hierarchy=hybrid)
[ 7.965395] systemd[1]: Detected architecture arm.
[ 8.045266] systemd[1]: Set hostname to <>.
[ 8.068268] systemd[1]: Hardware watchdog 'OMAP Watchdog', version 0
[ 8.076899] systemd[1]: Set hardware watchdog to 20s.
[ 9.998739] random: systemd: uninitialized urandom read (16 bytes read)
[ 10.007115] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ 10.043231] random: systemd: uninitialized urandom read (16 bytes read)
[ 10.062361] systemd[1]: Created slice System Slice.
[ 10.092491] random: systemd: uninitialized urandom read (16 bytes read)
[ 10.105719] systemd[1]: Created slice system-serial\x2dgetty.slice.
[ 10.145663] systemd[1]: Listening on Syslog Socket.
[ 10.184320] systemd[1]: Listening on Journal Socket.
[ 10.482495] random: crng init done
[ 10.487517] random: 7 urandom warning(s) missed due to ratelimiting
[ 12.519279] systemd-journald[81]: Received request to flush runtime journal from PID 1
[ 20.108488] CAN device driver interface
[ 20.743188] c_can_platform 481cc000.can: c_can_platform device registered (regs=baa7f7cc, irq=41)
[ 22.583761] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 23.055889] EXT4-fs (mmcblk1p3): mounted filesystem with ordered data mode. Opts: (null)
[ 23.248791] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 23.439278] omap-aes 53500000.aes: will run requests pump with realtime priority
[ 29.869212] net eth1: initializing cpsw version 1.12 (0)
[ 29.983004] NatSemi DP83620/DP83630/83640 Without PTP 4a101000.mdio:03: attached PHY driver [NatSemi DP83620/DP83630/83640 Without PTP] (mii_bus:phy_addr=4a101000.mdio:03, irq=POLL)
[ 29.986035] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
[ 37.075945] am335x-phy-driver 47401300.usb-phy: GPIO lookup for consumer reset
[ 37.075969] am335x-phy-driver 47401300.usb-phy: using device tree for GPIO lookup
[ 37.076014] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/usb@47400000/usb-phy@47401300[0]'
[ 37.076040] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp/usb@47400000/usb-phy@47401300[0]'
[ 37.076057] am335x-phy-driver 47401300.usb-phy: using lookup tables for GPIO lookup
[ 37.076070] am335x-phy-driver 47401300.usb-phy: No GPIO consumer reset found
[ 37.076083] am335x-phy-driver 47401300.usb-phy: GPIO lookup for consumer vbus-detect
[ 37.076092] am335x-phy-driver 47401300.usb-phy: using device tree for GPIO lookup
[ 37.076115] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpios' property of node '/ocp/usb@47400000/usb-phy@47401300[0]'
[ 37.076137] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpio' property of node '/ocp/usb@47400000/usb-phy@47401300[0]'
[ 37.076149] am335x-phy-driver 47401300.usb-phy: using lookup tables for GPIO lookup
[ 37.076159] am335x-phy-driver 47401300.usb-phy: No GPIO consumer vbus-detect found
[ 37.076516] am335x-phy-driver 47401300.usb-phy: Linked as a consumer to regulator.2
[ 37.217044] am335x-phy-driver 47401b00.usb-phy: GPIO lookup for consumer reset
[ 37.217069] am335x-phy-driver 47401b00.usb-phy: using device tree for GPIO lookup
[ 37.217123] of_get_named_gpiod_flags: can't parse 'reset-gpios' property of node '/ocp/usb@47400000/usb-phy@47401b00[0]'
[ 37.217148] of_get_named_gpiod_flags: can't parse 'reset-gpio' property of node '/ocp/usb@47400000/usb-phy@47401b00[0]'
[ 37.217167] am335x-phy-driver 47401b00.usb-phy: using lookup tables for GPIO lookup
[ 37.217180] am335x-phy-driver 47401b00.usb-phy: No GPIO consumer reset found
[ 37.217194] am335x-phy-driver 47401b00.usb-phy: GPIO lookup for consumer vbus-detect
[ 37.217203] am335x-phy-driver 47401b00.usb-phy: using device tree for GPIO lookup
[ 37.217226] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpios' property of node '/ocp/usb@47400000/usb-phy@47401b00[0]'
[ 37.217247] of_get_named_gpiod_flags: can't parse 'vbus-detect-gpio' property of node '/ocp/usb@47400000/usb-phy@47401b00[0]'
[ 37.217260] am335x-phy-driver 47401b00.usb-phy: using lookup tables for GPIO lookup
[ 37.217270] am335x-phy-driver 47401b00.usb-phy: No GPIO consumer vbus-detect found
[ 37.217623] am335x-phy-driver 47401b00.usb-phy: Linked as a consumer to regulator.2
[ 38.529858] usbcore: registered new interface driver usbfs
[ 38.529977] usbcore: registered new interface driver hub
[ 38.552789] usbcore: registered new device driver usb
[ 39.184765] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[ 39.184861] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
[ 39.245144] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19
[ 39.245170] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 39.245181] usb usb1: Product: MUSB HDRC host driver
[ 39.245192] usb usb1: Manufacturer: Linux 4.19.38 musb-hcd
[ 39.245202] usb usb1: SerialNumber: musb-hdrc.0
[ 39.253378] hub 1-0:1.0: USB hub found
[ 39.253539] hub 1-0:1.0: 1 port detected
[ 39.303383] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 39.303475] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
[ 39.311155] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 4.19
[ 39.311178] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 39.311189] usb usb2: Product: MUSB HDRC host driver
[ 39.311200] usb usb2: Manufacturer: Linux 4.19.38 musb-hcd
[ 39.311210] usb usb2: SerialNumber: musb-hdrc.1
[ 39.334449] hub 2-0:1.0: USB hub found
[ 39.359201] hub 2-0:1.0: 1 port detected
[ 39.822074] usb 2-1: new high-speed USB device number 2 using musb-hdrc
[ 40.002604] usb 2-1: New USB device found, idVendor=0451, idProduct=8142, bcdDevice= 1.00
[ 40.002628] usb 2-1: New USB device strings: Mfr=0, Product=0, SerialNumber=1
[ 40.002640] usb 2-1: SerialNumber: DB0000712C4B
[ 40.005172] hub 2-1:1.0: USB hub found
[ 40.005603] hub 2-1:1.0: 4 ports detected
[ 59.516099] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[ 59.645613] Bridge firewalling registered
[ 63.412216] Initializing XFRM netlink socket
[ 65.297560] IPv6: ADDRCONF(NETDEV_UP): docker0: link is not ready
[ 142.701749] usb 2-1.4: new high-speed USB device number 3 using musb-hdrc
[ 142.844960] usb 2-1.4: New USB device found, idVendor=3763, idProduct=3c93, bcdDevice= 3.18
[ 142.845000] usb 2-1.4: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 142.845022] usb 2-1.4: Product: Android
[ 142.845042] usb 2-1.4: Manufacturer: Android
[ 142.845063] usb 2-1.4: SerialNumber: 20ae3d01
[ 143.606949] usbcore: registered new interface driver option
[ 143.627659] usbserial: USB Serial support registered for GSM modem (1-port)
[ 143.628734] option 2-1.4:1.0: GSM modem (1-port) converter detected
[ 143.659818] usb 2-1.4: GSM modem (1-port) converter now attached to ttyUSB0
[ 143.685703] option 2-1.4:1.1: GSM modem (1-port) converter detected
[ 143.716096] usb 2-1.4: GSM modem (1-port) converter now attached to ttyUSB1
[ 143.754958] option 2-1.4:1.2: GSM modem (1-port) converter detected
[ 143.775886] usb 2-1.4: GSM modem (1-port) converter now attached to ttyUSB2
[ 143.823364] cdc_ether 2-1.4:1.3 usb0: register 'cdc_ether' at usb-musb-hdrc.1-1.4, CDC Ethernet Device, 7a:22:a9:af:4f:ad
[ 143.827125] option 2-1.4:1.5: GSM modem (1-port) converter detected
[ 143.827899] usb 2-1.4: GSM modem (1-port) converter now attached to ttyUSB3
[ 143.867902] usbcore: registered new interface driver cdc_ether
[ 149.993438] cdc_ether 2-1.4:1.3 lte0: renamed from usb0
Linux Kernel enumerate four ttyUSB and one CDC Ethernet Device, both devices working fine. lsusb info as follow:
root@test# lsusb
Bus 002 Device 005: ID 3763:3c93
Bus 002 Device 004: ID 0451:8142 Texas Instruments, Inc. TUSB8041 4-Port Hub
Bus 002 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
root@test# lsusb -t
/: Bus 02.Port 1: Dev 1, class="root_hub", Driver=musb-hdrc/1p, 480M
|__ Port 1: Dev 4, If 0, class="Hub", Driver=hub/4p, 480M
|__ Port 4: Dev 5, If 0, class="Vendor" Specific Class, Driver=option, 480M
|__ Port 4: Dev 5, If 1, class="Vendor" Specific Class, Driver=option, 480M
|__ Port 4: Dev 5, If 2, class="Vendor" Specific Class, Driver=option, 480M
|__ Port 4: Dev 5, If 3, class="Communications", Driver=cdc_ether, 480M
|__ Port 4: Dev 5, If 4, class="CDC" Data, Driver=cdc_ether, 480M
|__ Port 4: Dev 5, If 5, class="Vendor" Specific Class, Driver=option, 480M
/: Bus 01.Port 1: Dev 1, class="root_hub", Driver=musb-hdrc/1p, 480M
When I do this operation : power off (or unplug)LTE module when usb devices using, the kernel enter stop status. ttyO0 Console and networing stop , have no response , kernel heartbeat led stop flashing. Also dmesg don't print any more info about this errors.
But, in this status, I unplug TUSB4041 form AM3352 USB1, the kernel return to normal working immediately,heartbeat led start flashing. ttyO0 Console and networing return to work fine.dmesg also print usb disconnect info now.
[ 260.966850] usb 2-1: USB disconnect, device number 2
[ 260.966898] usb 2-1.4: USB disconnect, device number 3
[ 260.980230] option1 ttyUSB0: GSM modem (1-port) converter now disconnected from ttyUSB0
[ 260.980577] option 2-1.4:1.0: device disconnected
[ 260.988297] option1 ttyUSB1: GSM modem (1-port) converter now disconnected from ttyUSB1
[ 260.988598] option 2-1.4:1.1: device disconnected
[ 261.003237] option1 ttyUSB2: GSM modem (1-port) converter now disconnected from ttyUSB2
[ 261.003471] option 2-1.4:1.2: device disconnected
[ 261.004611] cdc_ether 2-1.4:1.3 lte0: unregister 'cdc_ether' usb-musb-hdrc.1-1.4, CDC Ethernet Device
[ 261.034563] option1 ttyUSB3: GSM modem (1-port) converter now disconnected from ttyUSB3
[ 261.034718] option 2-1.4:1.5: device disconnected
On this issue, I did two additional tests:
1)AM3352 + TUSB4041 + LTE module , Before power off the module , i do two steps:
1.dhcpcd -k usb0
2.close all opened ttyUSB device
After this operations, I power off the module, the kernel don't enter stop , eveything working fine, dmesg print usb disconnect info immediately:
[ 3298.326609] usb 2-1.4: USB disconnect, device number 5
[ 3298.332465] option1 ttyUSB0: GSM modem (1-port) converter now disconnected from ttyUSB0
[ 3298.332700] option 2-1.4:1.0: device disconnected
[ 3298.337618] option1 ttyUSB1: GSM modem (1-port) converter now disconnected from ttyUSB1
[ 3298.337788] option 2-1.4:1.1: device disconnected
[ 3298.343423] option1 ttyUSB2: GSM modem (1-port) converter now disconnected from ttyUSB2
[ 3298.343604] option 2-1.4:1.2: device disconnected
[ 3298.344022] cdc_ether 2-1.4:1.3 lte0: unregister 'cdc_ether' usb-musb-hdrc.1-1.4, CDC Ethernet Device
[ 3298.384089] option1 ttyUSB5: GSM modem (1-port) converter now disconnected from ttyUSB5
[ 3298.384243] option 2-1.4:1.5: device disconnected
and usb hub still working fine:
root@test# lsusb
Bus 002 Device 004: ID 0451:8142 Texas Instruments, Inc. TUSB8041 4-Port Hub
Bus 002 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
root@test# lsusb -t
/: Bus 02.Port 1: Dev 1, class="root_hub", Driver=musb-hdrc/1p, 480M
|__ Port 1: Dev 4, If 0, class="Hub", Driver=hub/4p, 480M
/: Bus 01.Port 1: Dev 1, class="root_hub", Driver=musb-hdrc/1p, 480M
2)AM3352 + LTE module , I connect LTE module direct to AM3352 USB1 with no usb hub,at this time, When USB devices working,I power off (or unplug)LTE module , kernel still working fine, don't enter stop , eveything working fine, dmesg print usb disconnect info immediately.
PS.I did all tests on PROCESSOR-SDK-LINUX-AM335X 06_00_00_07 , 05.03.00.07, 04.03.00.05, the same problem happened.
So, after doing these tests, My question is this a kernel driver bug, how can i fix it?