This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

can not root

hi

    please you tell me  that i have sucess the uimage,but i can not run in the demo board!  how to solve it ?

EVM # tftp 80700000 uImage-dm355

    EVM # nand erase 400000 200000

EVM # nand write 0x80700000 0x400000 0x200000

EVM # setenv bootcmd 'nboot 0x80700000 0 0x400000;bootm'

EVM # setenv bootargs 'console=ttyS0,115200n8 ip=dhcp

   root=/dev/mtdblock3 rw rootfstype=yaffs2 mem=116M'

U-Boot 1.2.0 (Feb  2 2008 - 23:52:10)

DRAM:  128 MB
NAND:  NAND device: Manufacturer ID: 0x2c, Chip ID: 0xd3 (Micron NAND 1GiB 3,3V 8-bit)
Bad block table found at page 524224, version 0x01
Bad block table found at page 524160, version 0x01
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xd3 (Micron NAND 1GiB 3,3V 8-bit)
Bad block table found at page 524224, version 0x01
Bad block table found at page 524160, version 0x01
2048 MiB
In:    serial
Out:   serial
Err:   serial
ARM Clock :- 216MHz
DDR Clock :- 171MHz
Hit any key to stop autoboot:  3  2  1  0

Loading from NAND 1GiB 3,3V 8-bit, offset 0x400000
   Image Name:   Linux-2.6.10_mvl401
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1638084 Bytes =  1.6 MB
   Load Address: 80008000
   Entry Point:  80008000
## Booting image at 80700000 ...
   Image Name:   Linux-2.6.10_mvl401
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1638084 Bytes =  1.6 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
OK

Starting kernel ...

Uncompressing Linux............................................................................................................. done, booting thek
Linux version 2.6.10_mvl401 (root@localhost.localdomain) (gcc version 3.4.3 (MontaVista 3.4.3-25.0.104.0600975 2006-07-06)) #1 Wed Jan 21 16:43:53 CST 2009
CPU: ARM926EJ-Sid(wb) [41069265] revision 5 (ARMv5TEJ)
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Machine: DaVinci DM355 EVM
Memory policy: ECC disabled, Data cache writeback
DM0350
Built 1 zonelists
Kernel command line: console=ttyS0,115200n8 ip=dhcp:eth0:off root=/dev/mtdblock3 rw rootfstype=yaffs2 mem=116M
PID hash table entries: 512 (order: 9, 8192 bytes)
Console: colour dummy device 80x30
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 116MB = 116MB total
Memory: 114048KB available (2868K code, 588K data, 168K init)
Mount-cache hash table entries: 512 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
spawn_desched_task(00000000)
desched cpu_callback 3/00000000
ksoftirqd started up.
desched cpu_callback 2/00000000
desched thread 0 started up.
NET: Registered protocol family 16
Registering platform device 'serial8250.0'. Parent at platform
Registering platform device 'nand_davinci.0'. Parent at platform
Registering platform device 'dm9000.0'. Parent at platform
Registering platform device 'mmc.0'. Parent at platform
Registering platform device 'mmc.1'. Parent at platform
DaVinci I2C DEBUG: 16:39:58 Jan 21 2009
Registering platform device 'i2c'. Parent at platform
SCSI subsystem initialized
usbcore: registered new driver usbfs
usbcore: registered new driver hub
musb_hdrc: version 2.2a/db-0.4.8 [cppi-dma] [host] [debug=0]
Registering platform device 'musb_hdrc'. Parent at platform
musb_hdrc: USB Host mode controller at c7800000 using DMA, IRQ 12
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
arch/arm/mach-davinci/spi_platform_init.c:dm355_spi_board_init:123 dm355_spi_board_init
arch/arm/mach-davinci/spi_platform_init.c:dm355_spi_board_init:129 REG BOARD  ret 0
Registering platform device 'dm_spi.0'. Parent at platform
arch/arm/mach-davinci/spi_platform_init.c:dm355_spi_board_init:136 REGISTER DEVICE ret 0
NetWinder Floating Point Emulator V0.97 (double precision)
NTFS driver 2.1.22 [Flags: R/O].
JFFS2 version 2.2. (NAND) (C) 2001-2003 Red Hat, Inc.
yaffs Jan 21 2009 16:39:10 Installing.
Initializing Cryptographic API
Registering platform device 'dm355fb.0'. Parent at platform
Console: switching to colour frame buffer device 90x30
watchdog: TI DaVinci Watchdog Timer: timer margin 64 sec
Registering platform device 'davinci_pwm0.0'. Parent at platform
Registering platform device 'davinci_pwm1.1'. Parent at platform
Registering platform device 'davinci_pwm2.2'. Parent at platform
Registering platform device 'davinci_pwm3.3'. Parent at platform
Serial: 8250/16550 driver $Revision: 1.90 $ 4 ports, IRQ sharing disabled
Registering platform device 'serial8250'. Parent at platform
ttyS0 at MMIO 0x1c20000 (irq = 40) is a 16550A
ttyS1 at MMIO 0x1c20400 (irq = 41) is a 16550A
ttyS2 at MMIO 0x1e06000 (irq = 14) is a 16550A
io scheduler noop registered
io scheduler anticipatory registered
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
loop: loaded (max 8 devices)
dm9000 Ethernet Driver
eth0: dm9000 at c7862000,c7864002 IRQ 45 MAC: 00:0e:99:02:c4:30
i2c /dev entries driver
Linux video capture interface: v1.00
Registering platform device 'vpfe.1'. Parent at platform
vpfe vpfe.1: DaVinci v4l2 capture driver V1.0 loaded
ipipe major#: 253, minor# 0
Registering platform device 'dm355_ipipe.2'. Parent at platform
ipipe driver registered
af major#: 252, minor# 0
Registering platform device 'dm355_af.2'. Parent at platform
aew major#: 251, minor# 0
Registering platform device 'dm355_aew.2'. Parent at platform
elevator: using anticipatory as default io scheduler
at25xxA_spi_eeprom init
nand_davinci nand_davinci.0: Using 4-bit hardware ECC
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xd3 (Micron NAND 1GiB 3,3V 8-bit)
2 NAND chips detected
nand_bbt: ECC error while reading bad block table
nand_bbt: ECC error while reading bad block table
Creating 5 MTD partitions on "nand_davinci.0":
0x00000000-0x003c0000 : "bootloader"
0x003c0000-0x00400000 : "params"
0x00400000-0x00800000 : "kernel"
0x00800000-0x20800000 : "filesystem1"
0x20800000-0x80000000 : "filesystem2"
nand_davinci nand_davinci.0: hardware revision: 2.3
scan_boardinfo:<NULL>:-1067628948
 modias <NULL> irq 2000000 max_speed 65535 bus_num 0 chip_select 0 mode -1068769520
drivers/spi/spi.cat25xxA_spi_eeprom device register Succeeded
dm_spi.0: dm355 SPI Controller driver at 0xc7866000 (irq = 42)
Initializing USB Mass Storage driver...
usbcore: registered new driver usb-storage
USB Mass Storage support registered.
usbcore: registered new driver usbhid
drivers/usb/input/hid-core.c: v2.0:USB HID core driver
Registering platform device 'hc.0'. Parent at platform
dummy_hcd hc.0: USB Host+Gadget Emulator, driver 29 Oct 2004
dummy_hcd hc.0: new USB bus registered, assigned bus number 2
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
mice: PS/2 mouse device common for all mice
mmc mmc.0: Supporting 4-bit mode
mmc mmc.0: Using DMA mode
mmc mmc.1: Supporting 4-bit mode
mmc mmc.1: Using DMA mode
Registering platform device 'davinci-audio.0'. Parent at platform
NET: Registered protocol family 2
IP: routing cache hash table of 512 buckets, 4Kbytes
TCP: Hash tables configured (established 8192 bind 16384)
Initializing XFRM netlink socket
NET: Registered protocol family 1
NET: Registered protocol family 10
IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
eth0: link down
IP-Config: Guessing netmask 255.0.0.0
IP-Config: Gateway not on directly connected network.
yaffs: dev is 32505859 name is "mtdblock3"
yaffs: Attempting MTD mount on 31.3, "mtdblock3"
block 2121 is bad
block 2574 is bad
eth0: link up, 100Mbps, full-duplex, lpa 0xC5E1
VFS: Mounted root (yaffs2 filesystem).
Freeing init memory: 168K
Warning: Cannot create /dev/console: -2Warning: unable to open an initial console.
Kernel panic - not syncing: No init found.  Try passing init= option to kernel.
 <7>eth0: no IPv6 routers present

  • I also  find the same problem.

    If I use the dm355_flash_image_1_30_01_41.tar from TI evm to store in the NAND FLASH,it will be ok.

    Then , I do

               1."tar -xf dm355_flash_image_1_30_01_41.tar ";

              2."rm  dm355_flash_image_1_30_01_41.tar "

              3."tar -cvf dm355_flash_image_1_30_01_41.tar  dm355_flash_image_1_30_01_41"

            4.I store the flash image to the flash

            5. The EVM boot failed.

  • The "Kernel panic - not syncing: No init found.  Try passing init= option to kernel" error is discussed in a few places on the forums, this error indicates that there is something corrupted or missing in your filesystem, the most common cause (and what I think is happening to you) is that somehow the symbolic links are not preserved somewhere along the line of getting the filesystem to the device. In this case I believe if you re tar the filesystem with the -h flag (so tar -cvfh ...) that you will avoid the no init found error.

  • I do it ,but if fail again.

    1."tar -cvfh dm355_flash_image_1_30_01_41"

    2.I get the file "h"

    3.I store it into flash,but it fail with the same indicates.

  • Can anyone please help me?

    How can I store my filesys into the Flash?

  • have you tried adding "noinitrd" option to bootargs

  • The bootargs is "setenv bootargs console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/mtdblock3 rw rootfstype=yaffs2 mem=80M video=davincifb:vid0=720x576x16,2500K:vid1=720x576x16,2500K:osd0=720x576x16,2025K davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=$(videostd)"

    Also ,I tried the bootargs "setenv bootargs console=ttyS0,115200n8 ip=dhcp root=/dev/mtdblock3 rw rootfstype=yaffs2 mem=80M video=davincifb:vid0=720x576x16,2500K:vid1=720x576x16,2500K:osd0=720x576x16,2025K davinci_enc_mngr.ch0_output=COMPOSITE davinci_enc_mngr.ch0_mode=$(videostd)".

    But ,all they failed.