Part Number: 66AK2G12
Dear All,
I have some questions related to the 66AK2G12 boot. I cannot find the missing information in the documentaion:
- Is the RBL also able to have the DSP core to be the boot master? With BOOTMODE pin 5 == 1?
- What is the DSP core counterpart for the ARMSS Boot RAM Memory Map (TRM 4.4)?
- In case of XIP boot the GPMC interface is used, isn't it?
- If so, how is it possible to give the RBL information about the required GPMC timing to access the connected memory chip? There are entries in the XIP boot parameter table (TRM 4.3.3.6 XIP Boot Parameter Table). But by default thy are not used (Options: Default Value 0). Is a multistage boot necessary for this?
- In a multistage boot I have to use more than one boot medium?
Kind Regards,
Bernhard