Other Parts Discussed in Thread: TMS320TCI6614
I read manuals KeyStone Architecture Viterbi Coprocessor (VCP2) and TMS320TCI6614 Communications Infrastructure KeyStone SoC but I didn't find information about max throughput and puncturing.
The TMS320TCI6614 device has four high-performance embedded Viterbi decoder coprocessors (VCP2) that significantly speed up channel-decoding operations on-chip. Each VCP2, operating at CPU clock divided-by-3, can decode more than 694 7.95-Kbps adaptive multi-rate (AMR) [K = 9, R = 1/3] voice channels. The VCP2 supports constraint lengths K = 5, 6, 7, 8, and 9, rates R = 3/4, 1/2, 1/3, 1/4, and 1/5, and flexible polynomials, while generating hard decisions or soft decisions.
Can I use the coprocessor for punctured code (e.g., r = 5/6)? And what is about max throughput for single channel? I wanna decode 54 Mbps. Is it possible?