Hi
I'd like to mount USB connector for USB3.0.
According to ch 3.3.11 of SERDES0 lane can be configured for USB3.0. Is it possible to get SERDES daughter cards which includes USB connect for USB3.0?
Best regards,
HaTa.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I'd like to mount USB connector for USB3.0.
According to ch 3.3.11 of SERDES0 lane can be configured for USB3.0. Is it possible to get SERDES daughter cards which includes USB connect for USB3.0?
Best regards,
HaTa.
Hi HaTa,
We do not sell the 1LanePCIE/USB3 serdes daughtercard separately. It is delivered with the TMDX654GPEVM while the TMDX654IDKEVM is delivered with the 2LanePCIE daughtercard.
Regards, Bill
Hi Bill,
Thank you very much, I understand.
So, it seems that USB3.0 host. Is it correct?
Is there USB3.0 device connector? (Is there any way to use USB3.0 device connector?)
Best regards.
HaTa.
Hi HaTa,
The USB3.0 connector on the USB3/1LanePCIE daughter card is a uAB connector that supports both host and device. There are some jumpers that will configure the connector to act as device and the correct software must be used but device is supported.
Regards, Bill