This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2SX: hciattach fail with the EMMY-W161 Module for Bluetooth

Part Number: TDA2SX

Hii -all,

We have an TDA2sx  board with EMMY-W161 module onboard, running Linux kernel 4.14 with BlueZ stack enabled.

We modified the UART port assignments for interfacing with the EMMY-W161 HCI UART lines, and tried various pinmux options enabling/disabling RTS/CTS.

When we use the TI-specific profile with 'hciattach', it switches HCI comm-link to faster baud rate with flow control enabled, but getting error like Unknown HCI packet type 00.

Here is the log,

root@dra7xx-evm:/opt/vision_sdk# hciattach /dev/ttyO6 any 3000000 flow
ps_init_work...
ps_init_timer...
ps_init...
Device setup complete
Unknown HCI packet type 00
Unknown HCI packet type 00
Unknown HCI packet type 00
Unknown HCI packet type 00
Unknown HCI packet type 00
Unknown HCI packet type 00
Unknown HCI packet type 00
Unknown HCI packet type 00
Unknown HCI packet type 00
Unknown HCI packet type 00