Part Number: AM5728
Hi,
Is there any AM5728 available for operating from -40C to 125C?
we have designed custom board with AM5728 Phytec SOM, the board has provision for capturing of three videos in which two has 1024x768 of resolution and one has 720x576 resolution.
we used TI EVM SDK for our application development. The custom consumes 28VDC@0.9A at root state and 28VDC@1.2A for processing of three videos (capturing, compression h.264 and streaming through ethernet at 100mbps).
My query is why it is consuming almost 30W when we pumping the power to custom board is 5VDC @75mA and 3.3VDC @3A.
The AM5728 SOC is heating up too fast junction temperature is 68C at 30C and 90C at 50 and thermal shutdown at 55C. Is there any way to resolve my issue.
We are compressing the data with H.264 compression default standard (2048kbps bitrate, high profile and level 40). To reduce the load on processor due to compression what are the changes and settings to be done.
Regards,
satya