Part Number: PROCESSOR-SDK-DRA8X
I'm trying to build the SDK filesystem per instructions here: http://swubn03.india.ti.com/publish/PROCESSOR-SDK-LINUX-AUTOMOTIVE/06_00_00_00/exports/docs/linux/Overview_Building_the_SDK.html
I've gotten to the last build step:
TOOLCHAIN_BASE=$HOME MACHINE=j7-evm bitbake -k arago-core-tisdk-image
At this step I get the following error, I've attached full log as well.
ERROR: quilt-native-0.65-r0 do_fetch: Build of do_fetch failed
My end goal is to run the cockpit demo:
1) Do I need the full SDK or will the target filesystem be sufficient?
2) I have the prebuilt SDK from my vision demo bring up - can I use this to run the cockpit demo?