hello !
I use dvsdk 2.00.00.22 , MV5.0 kernel 2.6.18 . The DDR RAM is 128MB on My board. but the config of DDR RAM in DVSDK 2.00.00.22 is 256MB.
so I need to change the memory map of dsplink.ko, and the demo " encodedecode " the map of loopback.x64P.
I donot know how to change them ! many files need to change. I try to change them many times ,but I am not ok.
becaue i run demo " encodedecode " is not ok . please tell me how to change thess files !!!!
my email : sanhaopu@163.com
[root@/opt/dm6446-2010-12-01]#./encodedecode -y 2 -O component -o
Encodedecode demo started.
<7><vpbe_encoder_enumoutput>
-------> davinci_enc_set_pal: test write start .....
-------> davinci_enc_set_pal: test write ended.
-------> davinci_enc_set_pal: test write start .....
-------> davinci_enc_set_pal: test write ended.
-------> davinci_enc_set_pal: test write start .....
-------> davinci_enc_set_pal: test write ended.
Error: Failed to create osd window device
Error: Failed to create UI
U-Boot 1.2.0 (Feb 11 2009 - 07:43:48)
dram_init info: start:0x80000000, size:0x8000000
DRAM: 128 MB NAND: 64 MB
In: serial
Out: serial
Err: serial
ARM Clock : 297MHz
DDR Clock : 135MHz
ETH PHY : BroadCom PHY Chip Hit any key to stop autoboot: 0