This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Make Binary BSP Run-Time-Image Error



 

 

Dear Experts,

@ OMAP35X and WinCE.

 

I got a Binary BSP and placed it to Platform\.

But when I "Make Run-Time-Image" ~ It got errors~!

Plz help ~ thx ~

 

===Below is compie msg======================================================================

------ Build started: Project: ADV_SOM_C3530, Configuration: ADV_SOM_C3530 ARMV4I Release Platform Builder (_TGTCPU) ------

Starting Build: makeimg

==============

makeimg for Windows CE (Release) (Built on Jul 10 2006 16:41:09)

makeimg: Change directory to C:\WINCE600.

 

makeimg: run command: cmd /C C:\WINCE600\public\common\oak\misc\pbpremakeimg

Generating PBWorkspace Custom makeimg build step batch Files to C:\WINCE600\OSDesigns\BSP_20101208\EVM_3530\EVM_3530\Wince600\ADV_SOM_C3530_ARMV4I\oak

Done Generating PBWorkspace Custom makeimg build step batch Files 

makeimg: Check for C:\WINCE600\OSDesigns\BSP_20101208\EVM_3530\EVM_3530\RelDir\ADV_SOM_C3530_ARMV4I_Release\PreMakeImg.bat to run.

makeimg: Found localization settings.

makeimg: LOCALE: 0409  LOCALE3: (null)  TargetDir: 0409  CodePage=1252  LocaleId: 409  PrimaryLandId: 9 SubLangId: 1

makeimg: Locale is 0409, retrieve files from usasnap directory.

makeimg: Moving files from usasnap to release...

makeimg: Read string substitutions from C:\WINCE600\OSDesigns\BSP_20101208\EVM_3530\EVM_3530\RelDir\ADV_SOM_C3530_ARMV4I_Release\intltrns\0409\

makeimg: Read string substitutions from C:\WINCE600\OSDesigns\BSP_20101208\EVM_3530\EVM_3530\RelDir\ADV_SOM_C3530_ARMV4I_Release\intltrns\0409\cebase.str

makeimg: Copy files from C:\WINCE600\OSDesigns\BSP_20101208\EVM_3530\EVM_3530\RelDir\ADV_SOM_C3530_ARMV4I_Release\intlfile\0409\ to release directory.

makeimg: Creating C:\WINCE600\OSDesigns\BSP_20101208\EVM_3530\EVM_3530\RelDir\ADV_SOM_C3530_ARMV4I_Release\nlscfg.out because C:\WINCE600\OSDesigns\BSP_20101208\EVM_3530\EVM_3530\RelDir\ADV_SOM_C3530_ARMV4I_Release\country.cfg doesn't exist or contains a locale different from 0409.

 

makeimg: run command: fmerge -nls C:\WINCE600\OSDesigns\BSP_20101208\EVM_3530\EVM_3530\RelDir\ADV_SOM_C3530_ARMV4I_Release\nlscfg.out C:\WINCE600\OSDesigns\BSP_20101208\EVM_3530\EVM_3530\RelDir\ADV_SOM_C3530_ARMV4I_Release\postproc\nlscfg.inf

fmerge for Windows CE (Release) (Built on Apr  5 2006 11:32:16)

 

makeimg: run command: fmerge -txt C:\WINCE600\OSDesigns\BSP_20101208\EVM_3530\EVM_3530\RelDir\ADV_SOM_C3530_ARMV4I_Release\postproc\nlssrc.txt C:\WINCE600\public\common\oak\files\locale.txt C:\WINCE600\OSDesigns\BSP_20101208\EVM_3530\EVM_3530\RelDir\ADV_SOM_C3530_ARMV4I_Release\nlssrc.txt

fmerge for Windows CE (Release) (Built on Apr  5 2006 11:32:16)

makeimg: FATAL ERROR: Command returned non-zero exit code 1 (dec).

makeimg: FATAL ERROR: Command returned non-zero exit code 1 (dec).

ADV_SOM_C3530 - 2 error(s), 0 warning(s)

========== Build: 0 succeeded or up-to-date, 1 failed, 0 skipped ==========

================================================================================