Hi,
we recently bought a AM335x Evaluation Module to start some research on working with TI´s SDK.
I have experienced the following using supplied linux SD card and with my own created with SDK 6.00.00.07.
While playing with the evaluation module I discovered an issue with the touchscreen. During the weston-calibration touch inputs are recognized, but after that the Matrix GUI does not response to touch inputs at all. I tried to re-calibrate several times using weston-calibration, but it did not work. However, weston-simple-touch seems to recognize touch inputs, so I can draw lines.
Am I missing some calibration steps to get it work?
Best Regards,
Sergej