This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5748: DSP1 restart error

Part Number: AM5748

Board: Custom board with AM5748

SDK: Custom linux based on meta-ti and meta-processor-sdk revisions for TI Processor SDK 5.02

Total system RAM: 512

There are two issues.

Issue 1. 

When dsp1 FW is first time started, we sometimes see this error:

[   21.909793] alloc_contig_range: [99800, 9ab00) PFNs busy

[   21.916997] alloc_contig_range: [99c00, 9ac00) PFNs busy

[   22.033134] cma: cma_alloc: alloc failed, req-size: 4096 pages, ret: -16

[   22.042204] omap-rproc 40800000.dsp: failed to allocate dma memory: len 0x1000000

[   22.051625] remoteproc remoteproc2: Failed to process resources: -12

[   22.079325] omap_hwmod: mmu0_dsp1: _wait_target_disable failed

[   22.098460] remoteproc remoteproc2: Boot failed: -12

[   22.103950] di-platform-start-apps.service: Started DSP processor ...

As per suggestion here: http://e2e.ti.com/support/processors/f/791/t/772040?Linux-AM5728-remoteproc-resource-failure-when-loading-DSP-firmware

we changed CMA allocation to "no-map" in DTS. This solved this problem.

        dsp1_memory_region: dsp1-memory@99000000 {

            compatible = "shared-dma-pool";

            reg = <0x0 0x99000000 0x0 0x4000000>;

            /* reusable; */

            no-map;

            status = "okay";

        };

But we continue to see below 2nd issue (again this happens sometimes only).

Issue 2. When re-start dsp1 FW, it fails with below errors:

[  153.613030] remoteproc remoteproc2: powering up 40800000.dsp

[  153.618919] LoadPin: firmware pinning-ignored obj="/mnt/data/APPROOT/bin/dra7-dsp1-fw.xe66" pid=1878 cmdline="/bin/bash /mnt/data/APPROOT/bin/start_apps.sh"

[  154.054961] remoteproc remoteproc2: Booting fw image dra7-dsp1-fw.xe66, size 20435816

[  154.062993] start_apps.sh: page allocation failure: order:2, mode:0x108c020(GFP_ATOMIC|__GFP_COMP|__GFP_ZERO), nodemask=(null)

[  154.078345] start_apps.sh cpuset=/ mems_allowed=0

[  154.083139] CPU: 0 PID: 1878 Comm: start_apps.sh Tainted: G           O    4.14.79-rt47-g28d73230da #1

[  154.083142] Hardware name: Generic DRA74X (Flattened Device Tree)

[  154.083145] Backtrace:

[  154.083164] [<c020bc60>] (dump_backtrace) from [<c020bf60>] (show_stack+0x18/0x1c)

[  154.083171]  r7:c1006620 r6:60080013 r5:00000000 r4:c105a538

[  154.083181] [<c020bf48>] (show_stack) from [<c09a7eac>] (dump_stack+0x90/0xa4)

[  154.083191] [<c09a7e1c>] (dump_stack) from [<c02f2e74>] (warn_alloc+0xe4/0x190)

[  154.083196]  r7:c1006620 r6:c0bb6fc4 r5:00000000 r4:c10064c8

[  154.083203] [<c02f2d94>] (warn_alloc) from [<c02f3dd8>] (__alloc_pages_nodemask+0xe08/0xfa8)

[  154.083207]  r3:00000002 r2:c0bb6fc4

[  154.083211]  r6:010ac020 r5:00000000 r4:00000000

[  154.083221] [<c02f2fd0>] (__alloc_pages_nodemask) from [<c0311b50>] (kmalloc_order+0x20/0x38)

[  154.083228]  r10:d16aca10 r9:00000000 r8:01088020 r7:c2e5e840 r6:c8270224 r5:d16aca10

[  154.083230]  r4:d17965c0

[  154.083240] [<c0311b30>] (kmalloc_order) from [<c0651a20>] (omap_iommu_attach_dev+0xfc/0x3a8)

[  154.083250] [<c0651924>] (omap_iommu_attach_dev) from [<c064ea20>] (__iommu_attach_device+0x4c/0x60)

[  154.083256]  r10:00000000 r9:d0585c20 r8:00000000 r7:d1787580 r6:c8270224 r5:d16aca10

[  154.083259]  r4:c8270224

[  154.083268] [<c064e9d4>] (__iommu_attach_device) from [<c064ea7c>] (__iommu_attach_group+0x48/0x70)

[  154.083272]  r5:d17875a8 r4:d17969c0

[  154.083279] [<c064ea34>] (__iommu_attach_group) from [<c064eb4c>] (iommu_attach_device+0x68/0xd4)

[  154.083284]  r7:d0585de4 r6:c8270224 r5:d17875b0 r4:d1787580

[  154.083309] [<c064eae4>] (iommu_attach_device) from [<bf063108>] (rproc_boot+0x36c/0x600 [remoteproc])

[  154.083314]  r7:d0585de4 r6:d0585ddc r5:c10064c8 r4:d0585c00

[  154.083343] [<bf062d9c>] (rproc_boot [remoteproc]) from [<bf064018>] (state_store+0x78/0x13c [remoteproc])

[  154.083349]  r10:d050c310 r9:c0033f68 r8:c3146940 r7:00000006 r6:d0585c00 r5:c3146940

[  154.083351]  r4:d0585c20

[  154.083371] [<bf063fa0>] (state_store [remoteproc]) from [<c06c69f0>] (dev_attr_store+0x20/0x2c)

[  154.083375]  r7:00000000 r6:00000000 r5:d050c300 r4:bf063fa0

[  154.083383] [<c06c69d0>] (dev_attr_store) from [<c03bebfc>] (sysfs_kf_write+0x40/0x4c)

[  154.083387]  r5:d050c300 r4:c06c69d0

[  154.083394] [<c03bebbc>] (sysfs_kf_write) from [<c03be344>] (kernfs_fop_write+0xe4/0x1c8)

[  154.083397]  r5:d050c300 r4:00000006

[  154.083405] [<c03be260>] (kernfs_fop_write) from [<c034e824>] (__vfs_write+0x40/0x14c)

[  154.083411]  r10:00000006 r9:024d3a10 r8:00000000 r7:c0033f68 r6:c82b6500 r5:c03be260

[  154.083414]  r4:c10064c8

[  154.083421] [<c034e7e4>] (__vfs_write) from [<c034eab4>] (vfs_write+0xac/0x170)

[  154.083426]  r10:00000006 r9:024d3a10 r8:00000000 r7:c0033f68 r6:024d3a10 r5:c82b6500

[  154.083428]  r4:00000006

[  154.083436] [<c034ea08>] (vfs_write) from [<c034ecbc>] (SyS_write+0x54/0xb4)

[  154.083441]  r9:024d3a10 r8:c82b6500 r7:00000000 r6:00000000 r5:c82b6500 r4:c10064c8

[  154.083450] [<c034ec68>] (SyS_write) from [<c020820c>] (__sys_trace_return+0x0/0x10)

[  154.083455]  r10:00000004 r9:c0032000 r8:c0208244 r7:00000004 r6:b6eedd98 r5:024d3a10

[  154.083457]  r4:00000006

[  154.083461] Mem-Info:

[  154.371722] active_anon:22452 inactive_anon:23978 isolated_anon:0

[  154.371722]  active_file:16773 inactive_file:14866 isolated_file:0

[  154.371722]  unevictable:0 dirty:169 writeback:0 unstable:0

[  154.371722]  slab_reclaimable:2049 slab_unreclaimable:4042

[  154.371722]  mapped:11913 shmem:24042 pagetables:354 bounce:0

[  154.371722]  free:22199 free_pcp:21 free_cma:21034

[  154.405676] Node 0 active_anon:89808kB inactive_anon:95912kB active_file:67092kB inactive_file:59464kB unevictable:0kB isolated(anon):0kB isolated(file):0kB mapped:47652kB dirty:680kB writeback:0kB shm

em:96168kB writeback_tmp:0kB unstable:0kB all_unreclaimable? no

[  154.429176] DMA free:88796kB min:2112kB low:2640kB high:3168kB active_anon:89808kB inactive_anon:95912kB active_file:66988kB inactive_file:59464kB unevictable:0kB writepending:680kB present:488448kB ma

naged:469560kB mlocked:0kB kernel_stack:1720kB pagetables:1416kB bounce:0kB free_pcp:84kB local_pcp:84kB free_cma:84136kB

[  154.457714] lowmem_reserve[]: 0 0 0 0

[  154.461414] DMA: 2073*4kB (UMEC) 1172*8kB (UMEC) 474*16kB (UMC) 640*32kB (UMC) 193*64kB (C) 35*128kB (C) 12*256kB (C) 1*512kB (C) 2*1024kB (C) 2*2048kB (C) 4*4096kB (C) = 88676kB

[  154.477491] 55687 total pagecache pages

[  154.481345] 0 pages in swap cache

[  154.484675] Swap cache stats: add 0, delete 0, find 0/0

[  154.489923] Free swap  = 0kB

[  154.492815] Total swap = 0kB

[  154.495708] 122112 pages RAM

[  154.498600] 0 pages HighMem/MovableOnly

[  154.503137] 4722 pages reserved

[  154.506291] 47104 pages cma reserved

[  154.509887] omap-rproc 40800000.dsp: failed to allocate required iommu data -12

[  154.517267] omap-rproc 40800000.dsp: can't attach iommu device: -12

[  154.523569] remoteproc remoteproc2: can't enable iommu: -12

[  154.545535] remoteproc remoteproc2: Boot failed: -12

How can we avoid this issue ?

dsp1 FW is restarted using:

echo stop > /sys/class/remoteproc/remoteproc2/state

echo start > /sys/class/remoteproc/remoteproc2/state