Part Number: 66AK2L06
Other Parts Discussed in Thread: RFSDK
We are Trying to set up 2 Antenna Containers with different sample sizes to obtain different PRI rates. We are using the RFSDK demo 1 configuration, and can successfully send out data on either Antenna container 0 or Antenna container 1, as long as the sample sizes are the same. Our application requires 2 different waveforms to be sent out at different times, with different PRI rates. If we change the sample size of Antenna container 1, we receive data but it seems to be shifted in the RX buffer. We are not sure if this is occurring on the ingress or egress portion. Should we be able to set up 2 antenna containers with different sample sizes in IQNET2, or do we require additional DFE configuration to accommadate different sample sizes.