Other Parts Discussed in Thread: OMAPL138
Hi,
I have an OMAPL138 based custom board and I am looking at the PRU CAN emulation from mistral. My problem is that I need to be able to have a bitrate of 250 kbit/sec on the CAN bus but when I read the release notes (0572.release_notes_soft-uart_linux_driver.zip) it says that the CAN bitrate is configurable to only 162.5 kbit/sec.
Is it possible to have 250kbit /sec bitrate with the PRU CAN emulation? My DSP is operating at 300MHz so I guess that the PRU is then operating at 150MHz?
// Henrik Abrahamsson