This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4376: LPDDR2 initialization issue

Part Number: AM4376

Hi SIr 

We used LPDDR2 with AM4376 for development.

Currently we used Micro LPDDR2 for development. It can boot successfully and work well.

And we changed the LPDDR2 to Nanya NT6TL256T32BQ-G0 and met some issues.

We used JTAG to connect with CPU by using below GEL setting. It can initialize well and do DDR_DataTransferCheck without error.

//********************************************************************************
// LPDDR2 Initialization
//********************************************************************************
//********************************************************************************
#define LPDDR2_ADDRCTRL_WD0_IOCTRL_VALUE 0x00000000 //no pullup/down on addr/ctrl
#define LPDDR2_ADDRCTRL_WD1_IOCTRL_VALUE 0x00000000 //no pullup/down on addr/ctrl
#define LPDDR2_ADDRCTRL_IOCTRL_VALUE 0x00000294 //Slew rate: fast, Impedance: 44ohms, no pullup/down
#define LPDDR2_DATA0_IOCTRL_VALUE 0x20000294 //Slew rate: fast, Impedance: 44ohms, pullup on DQSn, pulldown on DQS
#define LPDDR2_DATA1_IOCTRL_VALUE 0x20000294 //Slew rate: fast, Impedance: 44ohms, pullup on DQSn, pulldown on DQS
#define LPDDR2_DATA2_IOCTRL_VALUE 0x20000294 //Slew rate: fast, Impedance: 44ohms, pullup on DQSn, pulldown on DQS
#define LPDDR2_DATA3_IOCTRL_VALUE 0x20000294 //Slew rate: fast, Impedance: 44ohms, pullup on DQSn, pulldown on DQS

//timings for 266MHz LPDDR2 (8Gb)
#define LPDDR2_PHY_CTRL 0x0E288007

#define LPDDR2_SDRAM_TIMING1 0xEA86B411
#define LPDDR2_SDRAM_TIMING2 0x103A0E8A
#define LPDDR2_SDRAM_TIMING3 0x5F6BA22F
//#define LPDDR2_SDRAM_CONFIG 0x808052BA //16-bit LPDDR2
#define LPDDR2_SDRAM_CONFIG 0x80801AB2//0x808012BA //32-bit LPDDR2

#define LPDDR2_REF_CTRL 0x0000040D //266 * 3.9us = 0x40d
#define LPDDR2_ZQ_CONFIG 0x5007FA67

//===========================================================================//

After integrating above setting into MLO source code, it boots failed.

We cannot find the root cause and please advise 

Spec:NT6TL256T32BQ-G0.pdf

BR

Yimin