Part Number: AM5728
When I use the TIDL, there is a error which is weird. After the program runing a few seconds, the tiocl fatal error would be shown like following:
recvfrom failed: Link has been severed (67) rpmsgThreadFxn: transportGet failed on fd 24, returned -20 TIOCL FATAL: Communication to a DSP has been lost (likely due to an MMU fault). Please wait while the DSPs are reset and the runtime attempts to terminate. A reboot may be required before running another OpenCL application if this fails. See the kernel log for fault information.
So, why?
My program is like these.
tidl_set.h
#ifndef TIDL_SET_H
#define TIDL_SET_H
#include <QObject>
#include <QMetaType>
#include <QVariant>
//#include "configuration.h"
//#include "common/object_classes.h"
#include "common/utils.h"
#include "common/video_utils.h"
using namespace std;
using namespace tidl;
using namespace cv;
class Configuration;
class ObjectClasses;
typedef struct Result
{
cv::Mat image; //the image
uint32_t frame_index;
bool status; //success or fail
float time;
float ratio_xmin[20];
float ratio_ymin[20];
float ratio_xmax[20];
float ratio_ymax[20];
CvScalar color[20];
int index; //roi num
}result;
Q_DECLARE_METATYPE(result)
typedef struct Model_size
{
int width;
int height;
}model;
class TIDL_SET : public QObject
{
Q_OBJECT
public:
TIDL_SET();
~TIDL_SET();
public:
int dl_initial(int eve_num, int dsp_num, int orighight, int origwidth);
model dl_config();
bool dl_run(Mat bgr_frames[], int channel_size);
result dl_run_img();
void dl_set_threshold(uint32_t confidece_num);
signals:
void send_processed_image(QVariant variant);
//void send_processed_image(result resultdl);
public slots:
void dl_run_img1();
private:
bool WriteFrameOutput(const ExecutionObjectPipeline& eop,
const Configuration& c, const cmdline_opts_t& opts,
float confidence_value);
public:
// Process arguments
// Read the TI DL configuration file
Configuration c;
//Executor* e_dsp;
uint32_t pipeline_depth;
std::vector<ExecutionObjectPipeline *> eops;
uint32_t num_eops;
uint32_t frame_idx;
int orig_width;
int orig_height;
int channel_size;
float img_scale_h,img_scale_w;//to scale the outimage to original image
Mat bgr_frames[3];
//yes or not have image to process
volatile uint32_t have_image;
//the num of the processing_image for multi DSP
volatile uint32_t processing_image;
};
#endif // TIDL_SET_H
tild_set.cpp
#include "tidl_set.h"
#include "configuration.h"
#include "common/object_classes.h"
#include "executor.h"
#include "execution_object.h"
#include "execution_object_pipeline.h"
#include <signal.h>
#include <iostream>
#include <iomanip>
#include <fstream>
#include <cassert>
#include <functional>
#include <algorithm>
#include <time.h>
#include <unistd.h>
#include <queue>
#include <vector>
#include <cstdio>
#include <string>
#include <chrono>
#define NUM_VIDEO_FRAMES 100
#define DEFAULT_CONFIG "myjdetnet"
#define DEFAULT_INPUT "../test/testvecs/input/horse_768_320.y"
#define DEFAULT_INPUT_FRAMES (1)
#define DEFAULT_OBJECT_CLASSES_LIST_FILE "./barcode_objects.json"
#define DEFAULT_OUTPUT_PROB_THRESHOLD 40
Executor* CreateExecutor(DeviceType dt, uint32_t num, const Configuration& c,
int layers_group_id);
std::unique_ptr<ObjectClasses> object_classes;
cmdline_opts_t opts;
//static Executor* e_dsp;
/* Enable this macro to record individual output files and */
/* resized, cropped network input files */
//#define DEBUG_FILES
TIDL_SET::TIDL_SET()
{
orig_height=200;
orig_width=200;
frame_idx=0;
have_image = 0;
processing_image = 0;
}
TIDL_SET::~TIDL_SET()
{
//FreeMemory(eops);
//for (auto eop : eops) delete eop;
//delete e_dsp;
//delete e_eve;
}
int TIDL_SET::dl_initial(int eve_num, int dsp_num, int orighight, int origwidth)
{
// Process arguments
//cmdline_opts_t opts;
opts.config = DEFAULT_CONFIG;
opts.object_classes_list_file = DEFAULT_OBJECT_CLASSES_LIST_FILE;
opts.num_eves = eve_num;
opts.num_dsps = dsp_num;
opts.output_prob_threshold = DEFAULT_OUTPUT_PROB_THRESHOLD;
opts.num_frames=1;
opts.is_camera_input=0;
opts.is_video_input=0;
opts.is_preprocessed_input=0;
orig_width = origwidth;
orig_height = orighight;
// Get object classes list
object_classes = std::unique_ptr<ObjectClasses>(new ObjectClasses(opts.object_classes_list_file));
if (object_classes->GetNumClasses() == 0)
{
cout << "the file path is "<<opts.object_classes_list_file<<endl;
cout << "No object classes defined for this config." << endl;
return EXIT_FAILURE;
}
return 0;
}
model TIDL_SET::dl_config()
{
//read the config file
model model_size;
std::string config_file = "./tidl_config.txt";
bool status = c.ReadFromFile(config_file);
if (!status)
{
cerr << "Error in configuration file: " << config_file << endl;
model_size.height = -1;
model_size.width = -1;
return model_size;
}
img_scale_h = 1.0 / c.inHeight;
img_scale_w = 1.0 / c.inWidth;
channel_size = c.inHeight * c.inWidth;
qDebug("Scale_h = %f scale_w =%f",img_scale_h,img_scale_w);
model_size.height = c.inHeight;
model_size.width = c.inWidth;
return model_size;
}
void TIDL_SET::dl_run_img1()
{
try
{
Executor* e_dsp = CreateExecutor(DeviceType::DSP, opts.num_dsps,c,1);
std::vector<ExecutionObjectPipeline *> eops;
//set the depth of the pipeline
pipeline_depth = 1;
for (uint32_t j = 0; j < pipeline_depth; j++)
{
for (uint32_t i = 0; i < opts.num_dsps; i++)
{
eops.push_back(new ExecutionObjectPipeline({(*e_dsp)[i]}));
}
}
qDebug("lalalla");
num_eops = eops.size();
// Allocate input/output memory for each EOP
AllocateMemory(eops);
while(1)
{
if(have_image == 0 && processing_image == 0)
{
//qDebug("there isn't a image");
sleep(0.05);
continue;
}else{
qDebug("have_imgae = %d processing_image = %d", have_image, processing_image);
}
chrono::time_point<chrono::steady_clock> tloop0, tloop1,tloop2;
tloop0 = chrono::steady_clock::now();
result result_img;
result_img.index=0;
tloop2 = chrono::steady_clock::now();
// Process frames with available eops in a pipelined manner
// additional num_eops iterations to flush pipeline (epilogue)
ExecutionObjectPipeline* eop = eops[frame_idx % num_eops];
// Wait for previous frame on the same eop to finish processing
Mat frame, bgr[3];
qDebug("1111");
if (processing_image > 0)
{
if (eop->ProcessFrameWait())
{
qDebug("2222");
//WriteFrameOutput(*eop, c, opts, opts.output_prob_threshold);
//Mat frame, bgr[3];
int height= c.inHeight;
int width = c.inWidth;
unsigned char *in = (unsigned char *) eop->GetInputBufferPtr();
bgr[0] = Mat(height, width, CV_8UC(1), in);
bgr[1] = Mat(height, width, CV_8UC(1), in + channel_size);
bgr[2] = Mat(height, width, CV_8UC(1), in + channel_size*2);
cv::merge(bgr, 3, frame);
// Draw boxes around classified objects
float *out = (float *) eop->GetOutputBufferPtr();
int num_floats = eop->GetOutputBufferSizeInBytes() / sizeof(float);
for (int i = 0; i < num_floats / 7; i++)
{
int index = (int) out[i * 7 + 0];
if (index < 0) break;
float score = out[i * 7 + 2];
if (score * 100 < opts.output_prob_threshold) continue;
int label = (int) out[i * 7 + 1];
int xmin = (int) (out[i * 7 + 3] * width);
int ymin = (int) (out[i * 7 + 4] * height);
int xmax = (int) (out[i * 7 + 5] * width);
int ymax = (int) (out[i * 7 + 6] * height);
const ObjectClass& object_class = object_classes->At(label);
if(opts.verbose) {
printf("%2d: (%d, %d) -> (%d, %d): %s, score=%f\n",
i, xmin, ymin, xmax, ymax, object_class.label.c_str(), score);
}
if (xmin < 0) xmin = 0;
if (ymin < 0) ymin = 0;
if (xmax > width) xmax = width;
if (ymax > height) ymax = height;
cv::rectangle(frame, Point(xmin, ymin), Point(xmax, ymax),
Scalar(object_class.color.blue,
object_class.color.green,
object_class.color.red), 2);
result_img.ratio_xmin[result_img.index] = xmin * img_scale_w;//0.00390625;
result_img.ratio_ymin[result_img.index] = ymin * img_scale_h;//0.00390625;
result_img.ratio_xmax[result_img.index] = xmax * img_scale_w;//0.00390625;
result_img.ratio_ymax[result_img.index] = ymax * img_scale_h;//0.00390625;
result_img.color [result_img.index] = Scalar(object_class.color.blue,object_class.color.green,object_class.color.red);
result_img.index++;
}
result_img.image = frame;
result_img.frame_index = eop->GetFrameIndex();
result_img.status = true;
cv::imwrite("out.jpg",frame);
std::string name = eop->GetDeviceName();
qDebug("the name is %s", name.c_str());
QVariant variant;
variant.setValue(result_img);
tloop1 = chrono::steady_clock::now();
chrono::duration<float> elapsed = tloop1 - tloop0;
chrono::duration<float> elapsed1 = tloop1 - tloop2;
cout << "Loop total time (including read/write/opencv/print/etc): "
<< setw(6) << setprecision(4)
<< (elapsed.count() * 1000) << "ms" << endl;
cout << "run time: "
<< setw(6) << setprecision(4)
<< (elapsed1.count() * 1000) << "ms" << endl;
result_img.time = elapsed1.count()*1000;
emit send_processed_image(variant);
}
processing_image--;
}
if (have_image > 0)
{
char* frame_buffer = eop->GetInputBufferPtr();
memcpy(frame_buffer, bgr_frames[0].ptr(), channel_size);
memcpy(frame_buffer+1*channel_size, bgr_frames[1].ptr(), channel_size);
memcpy(frame_buffer+2*channel_size, bgr_frames[2].ptr(), channel_size);
eop->SetFrameIndex(frame_idx);
eop->ProcessFrameStartAsync();
frame_idx++;
processing_image++;
have_image--;
}
}//for while
FreeMemory(eops);
for (auto eop : eops) delete eop;
delete e_dsp;
}
catch (tidl::Exception &e)
{
cerr << e.what() << endl;
//result_img.status = false;
}
}
// Create frame with boxes drawn around classified objects
bool TIDL_SET::WriteFrameOutput(const ExecutionObjectPipeline& eop,
const Configuration& c, const cmdline_opts_t& opts,
float confidence_value)
{
// Asseembly original frame
int width = c.inWidth;
int height = c.inHeight;
int channel_size = width * height;
Mat frame, bgr[3];
unsigned char *in = (unsigned char *) eop.GetInputBufferPtr();
bgr[0] = Mat(height, width, CV_8UC(1), in);
bgr[1] = Mat(height, width, CV_8UC(1), in + channel_size);
bgr[2] = Mat(height, width, CV_8UC(1), in + channel_size*2);
cv::merge(bgr, 3, frame);
int frame_index = eop.GetFrameIndex();
char outfile_name[64];
// Draw boxes around classified objects
float *out = (float *) eop.GetOutputBufferPtr();
int num_floats = eop.GetOutputBufferSizeInBytes() / sizeof(float);
for (int i = 0; i < num_floats / 7; i++)
{
int index = (int) out[i * 7 + 0];
if (index < 0) break;
float score = out[i * 7 + 2];
if (score * 100 < confidence_value) continue;
int label = (int) out[i * 7 + 1];
int xmin = (int) (out[i * 7 + 3] * width);
int ymin = (int) (out[i * 7 + 4] * height);
int xmax = (int) (out[i * 7 + 5] * width);
int ymax = (int) (out[i * 7 + 6] * height);
const ObjectClass& object_class = object_classes->At(label);
if(opts.verbose) {
printf("%2d: (%d, %d) -> (%d, %d): %s, score=%f\n",
i, xmin, ymin, xmax, ymax, object_class.label.c_str(), score);
}
if (xmin < 0) xmin = 0;
if (ymin < 0) ymin = 0;
if (xmax > width) xmax = width;
if (ymax > height) ymax = height;
cv::rectangle(frame, Point(xmin, ymin), Point(xmax, ymax),
Scalar(object_class.color.blue,
object_class.color.green,
object_class.color.red), 2);
}
if (opts.is_camera_input || opts.is_video_input)
{
cv::imshow("SSD_Multibox", frame);
#ifdef DEBUG_FILES
// Image files can be converted into video using, example script
// (on desktop Ubuntu, with ffmpeg installed):
// ffmpeg -i multibox_%04d.png -vf "scale=(iw*sar)*max(768/(iw*sar)\,320/ih):ih*max(768/(iw*sar)\,320/ih), crop=768:320" -b:v 4000k out.mp4
// Update width 768, height 320, if necessary
snprintf(outfile_name, 64, "multibox_%04d.png", frame_index);
cv::imwrite(outfile_name, r_frame);
#endif
waitKey(1);
}
else
{
// Resize to output width/height, keep aspect ratio
Mat r_frame;
uint32_t output_width = opts.output_width;
if (output_width == 0) output_width = orig_width;
uint32_t output_height = (output_width*1.0f) / orig_width * orig_height;
cv::resize(frame, r_frame, Size(output_width, output_height));
snprintf(outfile_name, 64, "multibox_%d.png", frame_index);
cv::imwrite(outfile_name, frame);
printf("Saving frame %d with SSD multiboxes to: %s\n",
frame_index, outfile_name);
}
return true;
}
void TIDL_SET::dl_set_threshold(uint32_t confidece_num)
{
opts.output_prob_threshold = confidece_num;
}
// Create an Executor with the specified type and number of EOs
Executor* CreateExecutor(DeviceType dt, uint32_t num, const Configuration& c,
int layers_group_id)
{
if (num == 0) return nullptr;
DeviceIds ids;
for (uint32_t i = 0; i < num; i++)
ids.insert(static_cast<DeviceId>(i));
//return new Executor(dt, ids, c, layers_group_id);
printf("2222 \n");
return new Executor(dt, ids, c);
}
I wil use the dl_run_img1() function to process the image after the dl_initial() and dl_config. Please help me and my project has stuck here for a long time.