Part Number: AM5728
Hi,
My customer is using AM5728 on custom board.
On the board, PMIC(TPS6590379) POWERHOLD pin is used to control software power-down sequence.
- BOOT1 pin is pull-down (0)
- POWERHOLD pin is connected to AM5728 GPIO. The pin is driven to 0 when system wants to shut-down.
I understood our SDK does not support POWERHOLD.
Customer uses SDK Linux v03.03.00.04 based software and wants to know where they need to modify to enable POWERHOLD feature.
I found below E2E thread for similar topic.
https://e2e.ti.com/support/processors/f/791/p/765202/2829525
According to this thread,
- If BOOT1=0, DEV_ON bit needs to be set 0 and POWERHOLD pin is 0 to shut down the PMIC.
Is this only part customer should modify in SDK?
Thanks and regards,
Koichiro Tashiro