Part Number: AM4378
Hi Experts,
After USB_DRVVBUS is set as GPIO, it makes BUS OFF and ON.
If it is used as USB HOST, is it no problem not to use USB_DRVVBUS?
Thank you for your kind check.
Best regards,
HItoshi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM4378
Hi Experts,
After USB_DRVVBUS is set as GPIO, it makes BUS OFF and ON.
If it is used as USB HOST, is it no problem not to use USB_DRVVBUS?
Thank you for your kind check.
Best regards,
HItoshi
Hi Hitoshi-san,
Hitoshi Sugawara said:After USB_DRVVBUS is set as GPIO, it makes BUS OFF and ON.
No, it is not recommended to configure DRVVBUS pin in GPIO mode to control USB VBUS.
Hitoshi Sugawara said:If it is used as USB HOST, is it no problem not to use USB_DRVVBUS?
Yes, if the USB is in host-only mode, you can directly connect the USBx_VBUS pin to 5V power rail and not use USBx_DRVVBUS pin.
HI Bin,
Thank you for your kind clarification.
Will follow the advice.
Best regards,
Hioshi