Hello,
I ran QualiTI on my XDAIS algorithm. The following message was output:
Test failed. Problem: Not all external symbols declared by the module have the "<MODULE>_XXX_" prefix (i.e. module_vendor_).
The following is the list of offending symbols:
_llshr
_llshru
_llshl
_llshru
Nowhere in the algorithm source code is a reference to any of these symbols/functions, but I do use the C bit shift operators ('<<' and '>>') on various integer types including 'long long'. How can I get the algorithm XDAIS compliant (without QualiTI complaining)?
The algorithm was created with the GenAlg wizard included in XDAIS. The following is installed on my system (Windows XP Pro SP3):
Code Composer Studio v4.2.1.00004
xdais_7_20_00_07
C6000 Code Generation Tools 7.0.4
xdctools_3_21_00_27_eng
Thank you for your support.