This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/J6EVM5777: load using nor FLASH in J6-EVM but error

Part Number: J6EVM5777

Tool/software: Code Composer Studio

software : vision SDK 3.07

board: J6EVM(X5777)

i want to load using nor , and Reference resources is doc-- "VisionSDK_UserGuide_TDA2xx.pdf" in sdk

when i put sbl_nor_opp_high_a15_0_release.bin to board bu CCS, it is normal when i erase the nor flash and read file

/********************************************************************/

[CortexA15_0] Starting NOR Flash Writer.
CFI Query...passed.
NOR Initialization:
    Command Set: Spansion
    Manufacturer: SPANSION
    Size: 0x40 MB

Enter the file path to flash: DIR/sbl_nor_opp_high_a15_0_release.bin
Erasing the NOR Flash upto range: 0xC000000
Erased through 0x8020000
...
...
...
...
Erased through 0xC000000
Erase Completed
Load Options:
-------------
    0 -> fread using code (RTS Library)
    1 -> load raw using CCS (Scripting console)
Enter Load Option:
0
Reading 101316 bytes from file...
Read 16384 bytes [16%] from file...
Read 32768 bytes [32%] from file...
Read 49152 bytes [48%] from file...
Read 65536 bytes [64%] from file...
Read 81920 bytes [80%] from file...
Read 98304 bytes [97%] from file...
Read 101316 bytes [100%] from file. Done!!

/********************************************************************/

but when writing the data to nor flash, it is comes error as follows:

/********************************************************************/

Writing 0x18BC4bytes to NOR...
Data verify failed.

Buffered write failed @ address 0x%x
Trying normal write
Failed flashing @ 0x%x

Normal write also failed
NOR Write Failed...Aborting!
    ERROR: Writing NOR failed.
    NOR flashing failed!

/********************************************************************/