Hello, we are trying to prototype a medical device project that requires 1080p 30 encoding to h264.
I have gathered that
1. the dm6467T IC does this
2. the dm6467T EVAL BOARD does not do this due to an input capture problem
QUESTIONS:
1. Is there a dm6467T EVAL BOARD revision and/or daughterboard combo and/or CODEC revision that CAN capture and encode to h 264 at 1080p30 ??
Is it immediately available? We are using a REV C Eval Board, though it just crapped out. We need to buy another board for another developer too.
2. Is there an encode SAMPLE source-code using 1080p30 on the above hardware/software setup? Our managers are kind of freaking out about encoding claims without ways to demonstrate them. We need to do this in a short amount of time because to get the design win we have to do further customization.
We are using the DMAI 210, Davinci 3.10 community linux kit.