This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

No video playing out with TMX320DM365 Digital Video Evaluation Module Beta

Hi,

I followed the Setup Guide to test if the video was able to play out, but no video was playing out. I check the switch SW5 in "Setup Guide" and the online doc: http://processors.wiki.ti.com/index.php/GSG:_DM365_DVEVM_Hardware_Setup. There are different. The position 4 of SW5 in "Setup Guide" is on, but it is off in the online doc. I tried both, but none worked. My question is

1. Which one "on/off" to set in the position 4 of SW5?

2. Is my board broken? (If my board is broken, what should I do next? Is anyone I can contact to help me setting it up?)

Thanks for reply.

Best regards,

Bill