Hello,
I am interfacing a 14 bit CMOS sensor with a DM355 and would like to perform the following operation :
RAW DATA FROM SENSOR => RAW DATA IN SDRAM without any modification of those data.
I understand that IPIPE can be used to do this by setting the IPIPE_DPATHS.FMT to 2 (Raw to Boxcar mode).
However, where is the RAW data coming from to IPIPE ? Is it coming from the CCDC after the MEDIAN FILTER as describe in Fig 13 of SPRUF71A or is it possible for IPIPE to get the data directly from the Raw DATA pins of the DM355 ?
I am a bit lost and can't really find anything straightforward in dm355_ipipe.c and dm355_ccdc.c
Any help / recommendation on this would be highly appreciated...
Thank you very much
Kind regards,
Richard