This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI team,
I am looking for TI evaluation board based on primarily C674x (open to other TI DSP family as well like C55XX) SOC for audio processing applications in our project with following mandatory requirements :
1. Atleast 2 or more mic input interfaces.
2. USB powered only.
Can anyone help me find the right evaluation board based on above requirements.
Thanks and Regards,
Mohit
A small update : I am already able to find few evaluation board based on TMS320C6747 , TMS320C6748 but common misconception in technical documents
of both the above mentioned boards is that if they can be powered with USB alone ? This is the reason that it is difficult to found appropriate evaluation board for our needs.
Regards,
Mohit
Hi Mohit,
All available OMAP-L1x/TMS320C674x eval boards available on the market are listed here:
You could contact the vendors of these products to verify if they can be powered by USB only (if there are no schematics on the vendor's website).
Best Regards,
Yordan